Using i.MX as a Media Center, Audio Stream with S/PDIF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using i.MX as a Media Center, Audio Stream with S/PDIF

Jump to solution
2,601 Views
atillametetured
Contributor V

Hello

I am designing a multimedia centre using the imx6 and new to most of the stuff I come across with.

As part of the design I would like the card to support 5.1 and 7.1 home theater systems and for this

purpose, planning to use the S/PDIF interface that imx6 has.

Simply put my question is what intermediate ICs and devices do I need to connect in between my

home theather system and imx6 in case of;

     - Coaxial

     - Optical (TOSLINK)

When I give outputs from the Tx of the S/PDIF, how do I convert it to optical? If I use a coaxial connector

do I need nothing else but the cable in between? Obviously home theathre handles the DAC if it accepts

S/PDIF so that is not my problem.

A detailed explanation or guidance is welcome since I am completely new and self educated on the subject.

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
2,499 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

for convertion to optical one can use for example

GP1FAV30RK0F,GP1FMV31TK0F. Common description

can be found on:

https://en.wikipedia.org/wiki/S/PDIF

TOSLINK - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
2,500 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

for convertion to optical one can use for example

GP1FAV30RK0F,GP1FMV31TK0F. Common description

can be found on:

https://en.wikipedia.org/wiki/S/PDIF

TOSLINK - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,499 Views
atillametetured
Contributor V

Hello Igor,

Thanks for your reply. Just to make sure, please verify what I have in my mind.

Linux running on I.MX6  S/PDIF interface using a transmitter (GP1FMV31TK0F) connected

to a home theather system through an optical calbe (TOSLINK) will be a setup enough

to make it work (See attachment below for the Setup).

Best Regards,

Atilla

IMX6_SPDIF_Interface.jpg

0 Kudos
Reply
2,499 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes, this setup is enough to make it work.

~igor

0 Kudos
Reply
2,499 Views
atillametetured
Contributor V

Hi Igor,

Thank you.

Regards,

Atilla

0 Kudos
Reply