Using external RTC from SCFW in IMX8QXP based board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using external RTC from SCFW in IMX8QXP based board

1,922件の閲覧回数
_asif_muhammed_
Contributor III

Hi,

I have an external RTC on my custom board, which is connected to the SCU I2C. Could someone please confirm whether I can use it or not from SCFW?

Will I be only able to use the SNVS RTC from SCFW?

Will there be any internal driver which can communicate to an external RTC? Could someone please point me in the right direction?

@kerryzhou 

0 件の賞賛
返信
2 返答(返信)

1,901件の閲覧回数
_asif_muhammed_
Contributor III

Thank you Bio_TICFSL.I have gone through the document. It seems that it is an internal RTC of SNVS.

Is it possible to interface an external RTC to the SCU via the SCU_I2C?

0 件の賞賛
返信

1,906件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Should it be SC_R_SNVS (since that's where the RTC is located).  Please check it:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Timer-ser...

 

Regards

0 件の賞賛
返信