Using external RTC from SCFW in IMX8QXP based board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using external RTC from SCFW in IMX8QXP based board

1,872 次查看
_asif_muhammed_
Contributor III

Hi,

I have an external RTC on my custom board, which is connected to the SCU I2C. Could someone please confirm whether I can use it or not from SCFW?

Will I be only able to use the SNVS RTC from SCFW?

Will there be any internal driver which can communicate to an external RTC? Could someone please point me in the right direction?

@kerryzhou 

0 项奖励
回复
2 回复数

1,851 次查看
_asif_muhammed_
Contributor III

Thank you Bio_TICFSL.I have gone through the document. It seems that it is an internal RTC of SNVS.

Is it possible to interface an external RTC to the SCU via the SCU_I2C?

0 项奖励
回复

1,856 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Should it be SC_R_SNVS (since that's where the RTC is located).  Please check it:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Timer-ser...

 

Regards

0 项奖励
回复