Using eDMA for VPU en/decoding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using eDMA for VPU en/decoding

1,965 次查看
crg7475
Contributor III

Is it possible to use the eDMA for VPU en/decoding, specifically for transferring raw frames from/to the VPU? From what I see, the eDMA can do scatter-gather operations. This means it could in theory use virtual memory blocks (as long as they are located in the physical RAM and not paged to disk), because even if these are discontinuous in physical memory, the scatter-gather operation could read from the fragments. The big advantage would be that it would not be depending on the CMA, which is prone to fragmentation problems. But from what I recall, the eDMA is limited to some modules?

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,948 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

As far as i Know, the VPU of i.MX8 ha eDMA working for encode/ Decode.

Regards

0 项奖励
回复

1,946 次查看
crg7475
Contributor III

But then, is it set up to allow for scatter/gather operation? Could the VPU be set up to use system memory (which is fully resident in RAM) instead of having to allocate physically contiguous memory through CMA?

0 项奖励
回复