Using a iMx7 Sabre board and RGB888 works in UBoot but not linux.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using a iMx7 Sabre board and RGB888 works in UBoot but not linux.

924件の閲覧回数
stevetate
Contributor I

Using a iMx7 Sabre board I have fitted an RGB888 display and adapted the connector to suit. UBoot works and displays the freecsale logo and a small amount of text onto the LCD display,

But Yocto / Linux does not. The display just goes black and nothing is displayed. If I plug and HDMI display in then Linux displays the GUI on the Monitor correctly.  The LCD remains blank.

What have I missed, I have readd many docs but I am struggling to understand what the problem is.

I  would appreciate help,

Thanks  Steve T

0 件の賞賛
返信
1 返信

831件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

"UBoot works and displays the freecsale logo and a small amount of text onto the LCD display,

 

But Yocto / Linux does not."

 what do you mean? when the board boot up, you can see the freescale logo and text, then go to black and nothing??

could you share the log file ? any error message ?

0 件の賞賛
返信