Using a generic TFT display with Sabre Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a generic TFT display with Sabre Lite

Jump to solution
3,111 Views
davidbrooks
Contributor I

Hi all,

I am trying to understand how the parallel LCD display interface is used, from the Sabre Lite schematic.

That board was presumably designed with a particular (class of) display in mind: can someone tell me what it is? Then I'll get it's documentaion, & understand more.

Particularly, I need to understand better what these signals are used for:

PWM1 (pin 37)  - what does this do?

DRDY (pin 34)  - is this Data Enable?

CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Regards & thanks,

Labels (1)
0 Kudos
Reply
1 Solution
2,780 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

    I don't konw which schematic you are reading, but normally:

>>PWM1 (pin 37)  - what does this do?

this is PWM signal. there are more 2 PWM modules in i.MX SoC.

>>DRDY (pin 34)  - is this Data Enable?

This is data enable signal.

>>CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Yes, it is PWM signal. used to control back light of LCD.

Regards,

Weidong

View solution in original post

0 Kudos
Reply
3 Replies
2,781 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

    I don't konw which schematic you are reading, but normally:

>>PWM1 (pin 37)  - what does this do?

this is PWM signal. there are more 2 PWM modules in i.MX SoC.

>>DRDY (pin 34)  - is this Data Enable?

This is data enable signal.

>>CNTRST (pin 4) - this sounds like "contrast": is it a PWM signal?

Yes, it is PWM signal. used to control back light of LCD.

Regards,

Weidong

0 Kudos
Reply
2,780 Views
davidbrooks
Contributor I

Many thanks, Weidong.

I was using the Sabre Lite schematic published by Element 14 (aka Farnell Australia), Sheet 15.

Presumably the Sabre was designed with a particular display in mind (connector pinout, etc.) - do you know which that is?

Regards

0 Kudos
Reply
2,780 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,David,

       Please understand them like above what I described . and would you like to share schematic with me ?

my email : [email protected].

     

Thanks,

Weidong

0 Kudos
Reply