Using UART3_TXD (GPIO3[24]) as an GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using UART3_TXD (GPIO3[24]) as an GPIO

3,778 次查看
yonatanzvi
Contributor I

I'm using Variscite SOM-SOLO.

I cannot use UART3_TXD (GPIO3[24]) as an GPIO.

I can do that on UART2_TXD (GPIO3[26].

What could be the problem?

标签 (6)
标记 (3)
0 项奖励
回复
5 回复数

3,410 次查看
josephzhou1
Contributor V

see

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 项奖励
回复

3,567 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yonatan

seems on that board UART3 is used in DTE mode,

that is UART3_TXD is input and connected to output

U25 SN74AVC4T245 . Suggest to post that on

http://variwiki.com/index.php?title=Main_Page

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,568 次查看
yonatanzvi
Contributor I

Dear Igor,

As I understand, if we didn't change the DCEDTE control bit, it should be set as DCE (0), by default. No? So, actually, UART3_TXD had to act as an output. The pin is indeed acts as an output, it constantly set to 3.3V.

I also checked the RTS and CTE pins, to verify if we are in DCE or DTE mode. Seems that CTS acts as an output, which means we are in a DCE mode, no?

We also tried to modify the DCEDTE control bit, but seems that we have no control. CTS remained as an output, while RTS remained as an input.

Looks like something else is overruling our control.

0 项奖励
回复

3,568 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yonatan

problem is that output U25 SN74AVC4T245 is

connected to UART3 UART3_TXD, so whatever

mode you choses U25 will drive that signal, not UART.

~igor

0 项奖励
回复

3,568 次查看
yonatanzvi
Contributor I

Dear Igor,

Okay. So I understand I cannot do nothing with this signal.

I have to look for another alternatives, like CSI0_DAT14 (GPIO6[0]), to get my desired GPIO.

Many thanks for your support and prompt reply.

Yonatan

0 项奖励
回复