Using UART port on QSB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using UART port on QSB

3,456 次查看
VincentChou1z
Contributor III

Hi!  Friends,

Is there any step we could follow to use the RJ45 to connect to a module which we could control the module through UART?  Should we change the console parameter in the uboot environment so it will not interfere with our UART commands?

Vincent

标签 (1)
0 项奖励
回复
8 回复数

2,880 次查看
VincentChou1z
Contributor III

Hi! Serge, 

I created another account to login and then use "su root" to change user and it works.  Thanks anyway!

Vincent

0 项奖励
回复

2,880 次查看
Serge1z
Contributor II

Hi Vincent,

Actually you don't need to create another user to login on your PC. That can be needed only for security.

I guess it's better to allow of empty passwords.

/etc/ssh/sshd_config

PermitEmptyPasswords yes

Serge

0 项奖励
回复

2,880 次查看
VincentChou1z
Contributor III

Hi!  Serg,

I discovered that I need to create another user to use ssh on my PC to login to the target board.  Now the problem becomes how I could enable "sudo" in my target machine with the MIN profile configuration.  Could you provide me some idea?  Thanks!

Vincent

0 项奖励
回复

2,880 次查看
VincentChou1z
Contributor III

Hi! Serg,

I came across some strange ssh error and it shows

=============

The authenticity of host '10.1.1.112 (10.1.1.112)' can't be established.
RSA key fingerprint is 24:72:08:c9:45:7e:46:8b:cc:11:81:ec:90:65:55:64.
Are you sure you want to continue connecting (yes/no)? yes
Warning: Permanently added '10.1.1.112' (RSA) to the list of known hosts.
root@10.1.1.112's password:
Permission denied, please try again.
=============

However, I have already started dropbear when booted.  Is there anything I should set in order to login through SSH like this way?

I appreciate your help!

Vincent

0 项奖励
回复

2,880 次查看
Serge1z
Contributor II

My QSB sends to serial the following information:

U-Boot 2009.08 (Sep 24 2011 - 22:18:53)

CPU:   Freescale i.MX53 family 2.1V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 400MHz
mx53 pll3: 432MHz
mx53 pll4: 455MHz
ipg clock     : 66666666Hz
ipg per clock : 33333333Hz
uart clock    : 66666666Hz
cspi clock    : 108000000Hz
ahb clock     : 133333333Hz
axi_a clock   : 400000000Hz
axi_b clock   : 200000000Hz
emi_slow clock: 133333333Hz
ddr clock     : 400000000Hz
esdhc1 clock  : 80000000Hz
esdhc2 clock  : 80000000Hz
esdhc3 clock  : 80000000Hz
esdhc4 clock  : 80000000Hz
nfc clock     : 26666666Hz
Board: MX53-LOCO 1.0 Rev. B
Boot Reason: [WDOG]
Boot Device: SD
I2C:   ready
DRAM:   1 GB
MMC:   FSL_ESDHC: 0,FSL_ESDHC: 1
In:    serial
Out:   serial
Err:   serial
Serial reinitilized!
Net:   got MAC address from IIM: 00:04:9f:01:f5:76
FEC0 [PRIME]
Hit any key to stop autoboot:  0
mmc0 is current device

MMC read: dev # 0, block # 2048, count 6144 ... 6144 blocks read: OK
## Booting kernel from Legacy Image at 70800000 ...
   Image Name:   Linux-2.6.35.3-1129-g691c08a
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3008108 Bytes =  2.9 MB
   Load Address: 70008000
   Entry Point:  70008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Linux version 2.6.35.3-1129-g691c08a (root@serge-desktop) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #1 PREEMPT Fri Apr 6 21:01:20 MSK 2012
CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: Freescale MX53 LOCO Board
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 250880
Kernel command line: ip=192.168.10.24 root=/dev/mmcblk0p1 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 480MB 512MB = 992MB total
Memory: 998220k/998220k available, 17588k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xf9e00000 - 0xffe00000   (  96 MB)
    vmalloc : 0xe0800000 - 0xf4000000   ( 312 MB)
    lowmem  : 0x80000000 - 0xe0000000   (1536 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .init : 0x80008000 - 0x80033000   ( 172 kB)
      .text : 0x80033000 - 0x807fa000   (7964 kB)
      .data : 0x80818000 - 0x80870120   ( 353 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
        RCU-based detection of stalled CPUs is disabled.
        Verbose stalled-CPUs detection is disabled.
NR_IRQS:368
MXC GPIO hardware
MXC IRQ initialized
MXC_Early serial console at MMIO 0x53fbc000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
console [tty0] enabled, bootconsole disabled

I don't really know if it sends to each serial port or not (I don't have a special module for QSB).

If you find out how it works in detail, write here please.

Thanks for collaboration.

0 项奖励
回复

2,880 次查看
Serge1z
Contributor II

yes, you are right

but if this env parameter "console=ttymxc0,115200' is removed, as far as I remember some debug information from u-boot will be sent anyway

0 项奖励
回复

2,880 次查看
VincentChou1z
Contributor III

Thanks!  When you set ip=192.168.10.24 (assuming my ip is 192.168.10.24), is it going to specify the IP address only?  I remember there is an env parameter "console=ttymxc0,115200' in bootargs_base.  If we still keep that, we are going to see a lot of debug message output through the console.  Am I right?

0 项奖励
回复

2,880 次查看
Serge1z
Contributor II

you can try something like that:

setenv bootargs_mmc 'setenv bootargs ip=192.168.10.24 root=/dev/mmcblk0p1 rootwait rw'

192.168.10.24 is ip-addr of your QSB

also you are to install sshd and put it's name in autostart string... as far as I remember it is in /etc/rc.d/rc.conf


cfg_services="mount-proc-sys  udev hostname  depmod modules filesystems   inetd   sshd         "

cfg_services_r="         sshd   inetd   filesystems modules depmod  hostname udev  mount-proc-sys"

0 项奖励
回复