Using SWD/JTAG on MIMXRT1011-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SWD/JTAG on MIMXRT1011-EVK

2,810件の閲覧回数
gfisys
Contributor II

I can't seem to get SWD/JTAG via J-link Ultra to work on the MIMXRT1011-EVK. I've already removed jumpers J61 AND J62, when I initiate debug in MCUExpresso it throws this error message:

2023-04-09 07_44_38-workspace - evkmimxrt1010_igpio_led_output_source_gpio_led_output.c - MCUXpresso.png

Debugging with CMSIS-DAP works fine.

Can you advise? Thanks

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,809件の閲覧回数
gfisys
Contributor II

Forgot to mention, I connected the J-link to connector J55 on the EVK.

 

 

タグ(1)
0 件の賞賛
返信

2,790件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

Have you connect power to EVK?

 

Regards,

Jing

0 件の賞賛
返信

2,788件の閲覧回数
gfisys
Contributor II

Yes, I kept the CMSIS DAP usb connector (J41) plugged in to my PC and the board gets its power from that.

Am I supposed to use an external power supply instead? I didn't see anywhere that being a requirement for using external debugger/programmer.

 

 

0 件の賞賛
返信

2,776件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

I tested on my board, it works fine. You can compare the jumper. If nothing different, you can switch the board to serial download mode can check if the MCUBootUtlity can find RT1011. If yes, you can use MCUBootUtlity to erase the flash, then try to connect with jlink again.

jingpan_0-1681197818762.png

 

Regards,

Jing

0 件の賞賛
返信