Using SWD/JTAG on MIMXRT1011-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SWD/JTAG on MIMXRT1011-EVK

2,738 Views
gfisys
Contributor II

I can't seem to get SWD/JTAG via J-link Ultra to work on the MIMXRT1011-EVK. I've already removed jumpers J61 AND J62, when I initiate debug in MCUExpresso it throws this error message:

2023-04-09 07_44_38-workspace - evkmimxrt1010_igpio_led_output_source_gpio_led_output.c - MCUXpresso.png

Debugging with CMSIS-DAP works fine.

Can you advise? Thanks

Labels (1)
0 Kudos
Reply
4 Replies

2,737 Views
gfisys
Contributor II

Forgot to mention, I connected the J-link to connector J55 on the EVK.

 

 

Tags (1)
0 Kudos
Reply

2,718 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

Have you connect power to EVK?

 

Regards,

Jing

0 Kudos
Reply

2,716 Views
gfisys
Contributor II

Yes, I kept the CMSIS DAP usb connector (J41) plugged in to my PC and the board gets its power from that.

Am I supposed to use an external power supply instead? I didn't see anywhere that being a requirement for using external debugger/programmer.

 

 

0 Kudos
Reply

2,704 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @gfisys ,

I tested on my board, it works fine. You can compare the jumper. If nothing different, you can switch the board to serial download mode can check if the MCUBootUtlity can find RT1011. If yes, you can use MCUBootUtlity to erase the flash, then try to connect with jlink again.

jingpan_0-1681197818762.png

 

Regards,

Jing

0 Kudos
Reply