Using SSI, I2C, and an external audio codec with Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SSI, I2C, and an external audio codec with Linux

1,709件の閲覧回数
bobbyeshleman
Contributor I

I'm trying to use an on-board hardware codec with the i.MX6 Solo.  The wm8962 and hardware codec's driver are both configured for I2C.  Should the I2C subsystem be writing to the SSI controller's DMA address instead of the I2C device's address?

I've been referring to application note AN2629 (below), which leads me to believe that directly writing to the I2C device node's address is incorrect.

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Thanks.

タグ(4)
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer the link as below, hope helpful for you

https://community.nxp.com/thread/432057 

0 件の賞賛
返信