Using SSI, I2C, and an external audio codec with Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SSI, I2C, and an external audio codec with Linux

1,234 Views
bobbyeshleman
Contributor I

I'm trying to use an on-board hardware codec with the i.MX6 Solo.  The wm8962 and hardware codec's driver are both configured for I2C.  Should the I2C subsystem be writing to the SSI controller's DMA address instead of the I2C device's address?

I've been referring to application note AN2629 (below), which leads me to believe that directly writing to the I2C device node's address is incorrect.

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Thanks.

0 Kudos
Reply
1 Reply

1,085 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer the link as below, hope helpful for you

https://community.nxp.com/thread/432057 

0 Kudos
Reply