Using SRAM on SPI interface on IMX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using SRAM on SPI interface on IMX6UL

跳至解决方案
5,322 次查看
justinwave
Contributor I

Hello,

I have a custom board designed off the IMX6UL EVK board and what to access SRAM loacted on the SPI interface. The SRAM chip is the 23LC1024 and am using the 4.9.11_1.0.0_ga kernel. I was unable to find a driver for the SRAM and am unsure of how to configure it in the device tree and then how to read and write to it from user space.

In the device tree, what should I set the the compatible field to? Should it be "mtd-ram", "spidev" or "mmio-ram"?

Also, how then would I access the SRAM from a user space application?

Any help is greatly appreciated, thank you.

标签 (3)
0 项奖励
回复
1 解答
4,760 次查看
igorpadykov
NXP Employee
NXP Employee

Hi justinwave

one can look at general linux guidelines

F-RAM Support under Linux – KBA223028 | Cypress Developer Community 

[PATCH] mtd: mchp23k256: Add driver for this SPI SRAM device 

and NXP spi-nor driver description found in linux documentation on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,761 次查看
igorpadykov
NXP Employee
NXP Employee

Hi justinwave

one can look at general linux guidelines

F-RAM Support under Linux – KBA223028 | Cypress Developer Community 

[PATCH] mtd: mchp23k256: Add driver for this SPI SRAM device 

and NXP spi-nor driver description found in linux documentation on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,760 次查看
justinwave
Contributor I

Igor, thank you for the links. The patch for the mchp23k256 has been accepted and add to the mainline kernel. I was able to use this as a reference for a driver on the fsl 4.9 kernel.

Thank you.

0 项奖励
回复