Using OpenOCD with imx28evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using OpenOCD with imx28evk

Jump to solution
9,660 Views
tcmichals
Contributor III

All,

I'm trying to connect openOCD (Open On-Chip Debugger 0.6.1) to the imx28evk.  Is there some HW switches that need to configured?  Here is the output and command line:

sudo openocd -f interface/jtagkey-tiny.cfg -f board/imx28evk.cfg

Open On-Chip Debugger 0.6.1 (2012-10-27-10:53)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'jtag'

trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

dcc downloads are enabled

imx28evk_init

Error: An adapter speed is not selected in the init script. Insert a call to adapter_khz or jtag_rclk to proceed.

in procedure 'init'

tcmichals@tcmichals-RP829AV-ABA-d4790y:~$ sudo openocd -f interface/jtagkey-tiny.cfg -f board/imx28evk.cfg

Open On-Chip Debugger 0.6.1 (2012-10-27-10:53)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'jtag'

adapter speed: 10 kHz

trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain

adapter_nsrst_delay: 100

jtag_ntrst_delay: 100

dcc downloads are enabled

imx28evk_init

Info : clock speed 10 kHz

Error: JTAG scan chain interrogation failed: all ones

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: imx28.cpu: IR capture error; saw 0x0f not 0x01

Warn : Bypassing JTAG setup events due to errors

Info : Embedded ICE version 15

Error: unknown EmbeddedICE version (comms ctrl: 0xffffffff)

Info : imx28.cpu: hardware has 2 breakpoint/watchpoint units

Warn : WARNING: unknown debug reason: 0xf

Warn : ThumbEE -- incomplete support

Labels (1)
1 Solution
6,805 Views
tcmichals
Contributor III

OK figured it out, just read the map file...

                0x0000000000000000                . = 0x0

                0x0000000000000000                . = ALIGN (0x4)

.text           0x0000000040000100    0x2b11c

                0x0000000040000100                __image_copy_start = .

arch/arm/cpu/arm926ejs/start.o(.text)

.text          0x0000000040000100      0x480 arch/arm/cpu/arm926ejs/start.o

                0x0000000040000100                _start

So this translates to:

> load_image /home/tcmichals/Projects/Cygnetron/newProject/buildroot/cygBuildRoot/images/u-boot.bin 0x040000100

No working memory available. Specify -work-area-phys to target.

not enough working area available(requested 24)

no working area available, falling back to memory writes

250556 bytes written at address 0x40000100

downloaded 250556 bytes in 17.861929s (13.699 KiB/s)

> resume 0x040000100

>

Now u-boot does boot (Need to fix other issues ...)

View solution in original post

0 Kudos
Reply
6 Replies
6,805 Views
tcmichals
Contributor III

OK, it is connecting, I set the dip switches to JTAG mode. I do the following:

> load_image /home/tcmichals/Projects/Cygnetron/newProject/buildroot/cygBuildRoot/images/u-boot.bin

No working memory available. Specify -work-area-phys to target.

not enough working area available(requested 24)

no working area available, falling back to memory writes

250556 bytes written at address 0x00000000

downloaded 250556 bytes in 17.128075s (14.286 KiB/s)

> resume 0x41008000

Is the correct addresses?

0 Kudos
Reply
6,806 Views
tcmichals
Contributor III

OK figured it out, just read the map file...

                0x0000000000000000                . = 0x0

                0x0000000000000000                . = ALIGN (0x4)

.text           0x0000000040000100    0x2b11c

                0x0000000040000100                __image_copy_start = .

arch/arm/cpu/arm926ejs/start.o(.text)

.text          0x0000000040000100      0x480 arch/arm/cpu/arm926ejs/start.o

                0x0000000040000100                _start

So this translates to:

> load_image /home/tcmichals/Projects/Cygnetron/newProject/buildroot/cygBuildRoot/images/u-boot.bin 0x040000100

No working memory available. Specify -work-area-phys to target.

not enough working area available(requested 24)

no working area available, falling back to memory writes

250556 bytes written at address 0x40000100

downloaded 250556 bytes in 17.861929s (13.699 KiB/s)

> resume 0x040000100

>

Now u-boot does boot (Need to fix other issues ...)

0 Kudos
Reply
6,805 Views
anneshen
Contributor I

Hi Tim,

How did you fix your JTAG mode booting problem? I saw you had ERROR message below?

Info : clock speed 10 kHz

Error: JTAG scan chain interrogation failed: all ones

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: imx28.cpu: IR capture error; saw 0x0f not 0x01

Warn : Bypassing JTAG setup events due to errors

Info : Embedded ICE version 15

Error: unknown EmbeddedICE version (comms ctrl: 0xffffffff)

Info : imx28.cpu: hardware has 2 breakpoint/watchpoint units

Warn : WARNING: unknown debug reason: 0xf

Warn : ThumbEE -- incomplete support

Thanks,

Anne

0 Kudos
Reply
6,805 Views
ChristophG_Baum
Contributor III

Hello,

could you post your imx28.cfg and imx28evk.cfg? I'm trying the same as you did but it fails with this message: "memory write caused data abort (address: 0x47000000, size: 0x4, count: 0xe1f2)"

I'm also not sure if the imx28evk_init procedure is called correctly. I placed some echos in it which don't show up on starting openocd. When calling it later by hand I get complaints about the target being not halted despite the fact that openocd reported the target as halted on startup.

Do you have any hints?

Regards

Christoph

0 Kudos
Reply
6,805 Views
tcmichals
Contributor III

Sorry for the late reply, do still need help with this?  I'm currently using USB to load u-boot for unprogrammed parts..

0 Kudos
Reply
6,805 Views
ChristophG_Baum
Contributor III

The problem was that our platform does not have external regulators for 4.2V. So it relies entirely on the internal ones of the i.MX28. The start up script for the i.MX28EVK assumes that the regulators on the EVK are already powered.

Reading AN4199 chapter '3.1.3 4P2 Power Source' I came up with this OCD code to bring up the 4.2V supply:

#init 4P2 rail

#HW_POWER_DCDC4P2[TRG] = 0

#is reset state -> nothing to do

#HW_POWER_DCDC4P2[ENABLE_4P2] = 1

mww 0x80044080 0x00800018

sleep 20

#HW_POWER_DCDC4P2[ENABLE_4P2] = 1

mww 0x80044034 0x00400000

sleep 20

#HW_POWER_CHARGE[ENABLE_LOAD] = 1

mww 0x80044014 0x00001000

sleep 20

#HW_POWER_5VCTRL[PWD_CHARGE_4P2] = 0

mww 0x80044018 0x00300000

sleep 20

#HW_POWER_DCDC4P2[ENABLE_DCDC] = 1

mww 0x80044080 0x00C00018

sleep 20

#charge 4p2 cap

#step up HW_POWER_5VCTRL[CHARGE_4P2_ILIMIT]

mww 0x80044014 0x00002000

sleep 1

mww 0x80044014 0x00004000

sleep 1

mww 0x80044014 0x00008000

sleep 1

mww 0x80044014 0x00010000

sleep 1

mww 0x80044014 0x00020000

sleep 20

After that the initialization can continue with the script as it is in OpenOCD.