Using IMX-MIPI-HDMI with imx93-evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using IMX-MIPI-HDMI with imx93-evk

7,857件の閲覧回数
dpcivl
Contributor III

Hi, I'm setting my imx93-evk board to see how the camera is well working.

I bought IMX-MIPI-HDMI to watch the frame from the camera with HDMI monitor.

However, even after I connected the board to the monitor, the monitor displays nothing.
(LEDs on IMX-MIPI-HDMI are on - yellow and red)

Should I edit some U-boot settings?

If I should, please let me know. 

 

+) I read this page and I followed U-boot Steps.  https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Build-GUI-Guider-projects-for-iMX93-BSP-...

But the result is the same. 

タグ(2)
0 件の賞賛
返信
9 返答(返信)

7,834件の閲覧回数
dpcivl
Contributor III

I found U-boot configuration could be shown on display. 

But after finishing configuration, the monitor is shut down immediately. 

How can I fix it? 🥲

0 件の賞賛
返信

7,831件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you use nxp evk board? what did you change? what dtb file do you use?

0 件の賞賛
返信

7,826件の閲覧回数
dpcivl
Contributor III
Yes, I'm using i.MX93EVK. I changed U-boot configuration about fdtfile. I'm using imx93-11x11-evk-rm67199.dtb now. I don't have an idea about which dtb file I should select.
0 件の賞賛
返信

7,812件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you don't need change any fdt file, you just use the default dtb, which isimx93-11x11-evk.dtb, the dtb you choose if for mipi display, not for hdmi

0 件の賞賛
返信

7,795件の閲覧回数
dpcivl
Contributor III
I've tried with another HDMI monitor and it displayed well. I think this is about the resolution of the former monitor, not about dtb file. So I want to know how I can config the resolution of DSI port so as to try again with the former monitor. Could you tell me?
0 件の賞賛
返信

7,774件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean you can boot up new hdmi display even use imx93-11x11-evk-rm67199.dtb? what old hdmi display resolution and pixel clock you use? current bsp uses adv7535 as mipi to hdmi bridge, if your hdmi clock isn't supported by adv7535, you need add new clock in the clock driver, but imx93-11x11-evk-rm67199.dtb deleted the adv7535, so if you want to bring up mipi to hdmi, you need use imx93-11x11-evk.dtb

0 件の賞賛
返信

7,725件の閲覧回数
dpcivl
Contributor III
I meant that the monitor B worked well with imx93-11x11-evk.dtb. But I got a problem with the monitor A which was used when my first trial. The monitor A doesn't work well though I set dtb file to imx93-11x11-evk.dtb.

So I want to know how to configure resolution for using the monitor A correctly. If there is no way to edit resolution setting, I will use the monitor B which works well with no setting for the resolution.

+) I don't know the resolution and pixel clock of the monitor A. Sorry about that.
0 件の賞賛
返信

7,716件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

ok got it, because you said not the dtb issue, so I need double confirm, firstly you need choose the correct dtb file, then you need to know what pixel clock of your display you need support, then you can add in the source code, maybe you can check the logfile, can to check if any information about your monitorA, or use cat /sys/module/drm/parameters/ to check it

0 件の賞賛
返信

7,169件の閲覧回数
peterdoliwa
NXP Employee
NXP Employee

Hi, I have a similar issue, I also have an IMX-MIPI-HDMI connected to my imx93-evk and my monitor works in uboot, but only shows a black screen after full boot to linux. I'm using the default dtb file. Could you provide some details how to debug this kind of issues and find out the monitor configuration? Thx

0 件の賞賛
返信