Using I.MX8QuadMax for deep learning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using I.MX8QuadMax for deep learning

2,068件の閲覧回数
Param21
Contributor II

I want to install Tensorflow and other required libraries like mediapipe, opencv and tensorflow hub in I.MX8QuadMax for a deep learning based application which utilizes camera. How can i install my these requirements easily on the linux image of I.MX8QuadMax.

0 件の賞賛
返信
4 返答(返信)

2,034件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

OpenCV, Tensorflow lite should be already integrated with BSP, and you can pip install for mediapipe.

More details, please refer to IMX-MACHINE-LEARNING-UG.pdf 

 

Regards

Harvey

2,027件の閲覧回数
Param21
Contributor II

Thank you so much for your response and can you please answer the following questions:


which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?

How to include tensorflow Hub since my project uses tensorflow hub APIs as well?

Does I.MX8QuadMax kit comes with inbuilt Wi-Fi support?

0 件の賞賛
返信

1,984件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

There is no in-built WiFi, interface M.2 KEY E available though.

Regards

Harvey

0 件の賞賛
返信

2,024件の閲覧回数
Param21
Contributor II
which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?
this query is solved. please reply for the remaining two questions.
0 件の賞賛
返信