Using I.MX8QuadMax for deep learning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using I.MX8QuadMax for deep learning

2,142 Views
Param21
Contributor II

I want to install Tensorflow and other required libraries like mediapipe, opencv and tensorflow hub in I.MX8QuadMax for a deep learning based application which utilizes camera. How can i install my these requirements easily on the linux image of I.MX8QuadMax.

0 Kudos
Reply
4 Replies

2,108 Views
Harvey021
NXP TechSupport
NXP TechSupport

OpenCV, Tensorflow lite should be already integrated with BSP, and you can pip install for mediapipe.

More details, please refer to IMX-MACHINE-LEARNING-UG.pdf 

 

Regards

Harvey

2,101 Views
Param21
Contributor II

Thank you so much for your response and can you please answer the following questions:


which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?

How to include tensorflow Hub since my project uses tensorflow hub APIs as well?

Does I.MX8QuadMax kit comes with inbuilt Wi-Fi support?

0 Kudos
Reply

2,058 Views
Harvey021
NXP TechSupport
NXP TechSupport

There is no in-built WiFi, interface M.2 KEY E available though.

Regards

Harvey

0 Kudos
Reply

2,098 Views
Param21
Contributor II
which version of linux image to be downloaded from the NXP website which includes all these libraries and it is ready to use for the application for I.MX8QuadMax?
this query is solved. please reply for the remaining two questions.
0 Kudos
Reply