Using GPU on IMX-8qxp for CNN Inference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using GPU on IMX-8qxp for CNN Inference

1,459 Views
parag_jain
Contributor I

Context :

I would like to inference my CNN model on IMX-8qxp unit. As your website states, inference is supported on Vulkan GPU on IMX-8qxp through eIQ for ARM-NN & TF-Lite models(https://www.nxp.com/docs/en/fact-sheet/EIQ-FS.pdf )[Page-2] . Following are the related questions. 

Questions :

1) IMX-8qxp has 1x4-shader Vulkan GPU. Can we access this GPU using latest eIQ package for CNN model inference? 
2) If yes, would you please share some reference documents? 
3) If GPU based CNN inference is supported, can we use eIQ as stand-alone module or does it BSP to be rebuilt? 
4) GpuAcc flag in ARM-NN supports only Mali-based GPU. Can you please point me to a sample C++ testapp in which eIQ is used for inference on Vulkan GPU?

0 Kudos
Reply
1 Reply

1,439 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello parag,

 

1. The MX8X has the GPU7000Lite but not have NPU. the eIQ that can access is on L5.4.70.

2. The eIQ documents are in your yocto relases.

3. Is in the L5.4.70 BSP

4. you can download the demos from https://github.com/NXPmicro/gtec-demo-framework

 

Regards

 

0 Kudos
Reply