Using Dual-LVDS I/F and RGB I/F by 2Display system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using Dual-LVDS I/F and RGB I/F by 2Display system

2,079 次查看
takashitakahash
Contributor III

Use the iMX6 Dual, we would like to drive the TFT resolution of 1920x720 and 800x480 resolution TFT resolution at the same time and same contents.

There are TFT interface, the 1920 x 720 are  Dual-LVDS and 800 x 480 are RGB24bit .

connection with iMX6 is connected to Dual-LVDS are LVDS0, 1 and RGB24bit are connected to the IPU1_DISP0.

At this time, 2 CH of the IPU Display I/f (DI) is assigned Dual-LVDS and RGB24bit each ?

In other words, Dual-LVDS data (DI), after entered into LVDS Display Bridge (LDB), divided by  even pixels and odd pixels after output from LVDS0 and LVDS1.

In my understand is correct ?

标签 (1)
0 项奖励
回复
2 回复数

1,447 次查看
joanxie
NXP TechSupport
NXP TechSupport

how to assign the DI depends on what lvds mode you use, single, Separate,dual, split.

more detailed information, you can refe to the Table 39-5. Channel Mapping of mx6 Reference Manual.

Mapping of Parallel input interfaces (DI0, DI1) to output LVDS channels (Channel 0,

Channel 1).

0 项奖励
回复

1,447 次查看
zhouli
Contributor II

So and i

0 项奖励
回复