Using DMA transfer data from memory to SATA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using DMA transfer data from memory to SATA

2,918 Views
sharpjison
Contributor II

Hello NXP:

      In kernel space, I need to use DMA to transfer a big data from DDR to SATA .

      This operation is nothing to do with using space and the file system.

       What can I refer to?

 

Have a nice day!

Thanks !

Labels (3)
0 Kudos
Reply
1 Reply

2,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

sdma is supported in nxp linux for some modules and described in Chapter 4 Smart

Direct Memory Access (SDMA) API attached Linux Manual. Unfortunately there

is no such support and sdma script for sata. In general one can try to reuse approach

for pcie (IPU used as the bus master(DMA)) from link

i.MX6Q PCIe EP/RC Validation System 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply