Using DATA3 as cd pin in SD card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using DATA3 as cd pin in SD card

4,386件の閲覧回数
Robbi
Contributor III

Hi team,

                 I'm working with i.MX91 custom board, the major difference in SD Card interface is EVK is using dedicated GPIO for card detection, but we are using DATA3. I changed Kernel dts file as (Mentioned in RM DATA3 should be pull-down)

&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
pinctrl-0 = <&pinctrl_usdhc2>;
pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
pinctrl-3 = <&pinctrl_usdhc2_sleep>;
cd-gpios = <0>;
fsl,cd-gpio-wakeup-disable;
fsl,cd-controller;
bus-width = <4>;
status = "okay";
no-sdio;
};
 
 
 
and iomux:
pinctrl_usdhc2: usdhc2grp {
fsl,pins = <
MX91_PAD_SD2_CLK__USDHC2_CLK 0x1582
MX91_PAD_SD2_CMD__USDHC2_CMD 0x1382
MX91_PAD_SD2_DATA0__USDHC2_DATA0 0x1382
MX91_PAD_SD2_DATA1__USDHC2_DATA1 0x1382
MX91_PAD_SD2_DATA2__USDHC2_DATA2 0x1382
MX91_PAD_SD2_DATA3__USDHC2_DATA3 0x1582
 
>;
};

pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp {
fsl,pins = <
MX91_PAD_SD2_CLK__USDHC2_CLK 0x158e
MX91_PAD_SD2_CMD__USDHC2_CMD 0x138e
MX91_PAD_SD2_DATA0__USDHC2_DATA0 0x138e
MX91_PAD_SD2_DATA1__USDHC2_DATA1 0x138e
MX91_PAD_SD2_DATA2__USDHC2_DATA2 0x138e
MX91_PAD_SD2_DATA3__USDHC2_DATA3 0x158e
>;
};

pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp {
fsl,pins = <
MX91_PAD_SD2_CLK__USDHC2_CLK 0x15fe
MX91_PAD_SD2_CMD__USDHC2_CMD 0x13fe
MX91_PAD_SD2_DATA0__USDHC2_DATA0 0x13fe
MX91_PAD_SD2_DATA1__USDHC2_DATA1 0x13fe
MX91_PAD_SD2_DATA2__USDHC2_DATA2 0x13fe
MX91_PAD_SD2_DATA3__USDHC2_DATA3 0x15fe
 
>;
};

pinctrl_usdhc2_sleep: usdhc2grpsleep {
fsl,pins = <
MX91_PAD_SD2_CLK__GPIO3_IO1 0x51e
MX91_PAD_SD2_CMD__GPIO3_IO2 0x51e
MX91_PAD_SD2_DATA0__GPIO3_IO3 0x51e
MX91_PAD_SD2_DATA1__GPIO3_IO4 0x51e
MX91_PAD_SD2_DATA2__GPIO3_IO5 0x51e
MX91_PAD_SD2_DATA3__GPIO3_IO6 0x51e
>;
};
 
 
slight changes are done, but after power-up, SPL unable to detect MMC1. Kindly help me to sort the issue.
 
Thanks.
0 件の賞賛
返信
8 返答(返信)

4,355件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @Robbi!
Thank you for contacting NXP Support!

 

The configuration that I recommend is the next:

&usdhc2 {
    pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
    pinctrl-0 = <&pinctrl_usdhc2>;
    pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
    pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
    pinctrl-3 = <&pinctrl_usdhc2_sleep>;
    fsl,cd-gpio-wakeup-disable;
    fsl,cd-controller;
    bus-width = <4>;
    status = "okay";
    no-sdio;
};

 

The pinctrl looks good.

Do you want to boot from SD card using usdhc2?

This device tree is the u-boot device tree or Linux-device tree?

 

What BSP version are you using?

 

Best Regards!

Chavira

0 件の賞賛
返信

4,307件の閲覧回数
Robbi
Contributor III

Hi @Chavira ,

Please suggest me what changes need to be done, to boot from sd card.

0 件の賞賛
返信

4,338件の閲覧回数
Robbi
Contributor III

Thanks @Chavira ,

For the response, this kernel dts, initially I left u-boot dts same as imx91 EVK but later I tried and changed. still same error MMC1 not detecting.

  1. Is this same dts node should be in u-boot dts?
  2. Any other files need to be modified.

Thanks.

Robbi

0 件の賞賛
返信

4,294件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @Robbi!

 

Yes the changes should be done in U-boot device tree too.

Can you share the schematic of the SD connections?

 

Best Regards!

Chavira

0 件の賞賛
返信

4,287件の閲覧回数
Robbi
Contributor III

Please find the attached image.

SD_CARD.png

 And the interface of pins with IMX91, where SD2_CD_B is not used.

[AA19] SD2_CLK SD2_CLK
[Y19] SD2_CMD SD2_CMD
[Y18] SD2_DATA0 SD2_DATA0
[AA18] SD2_DATA1 SD2_DATA1
[Y20] SD2_DATA2 SD2_DATA2
[AA20] SD2_DATA3 SD2_DATA3
[AA17] SD2_RESET_BSD2_nRST

Thanks

Robbi

0 件の賞賛
返信

4,256件の閲覧回数
Robbi
Contributor III

Robbi_0-1747137825710.png

And while booting from emmc try to detect using lsblk command, but unable to find, displays error above message 

 

0 件の賞賛
返信

4,336件の閲覧回数
Robbi
Contributor III
BSP = 6.6.52
0 件の賞賛
返信

4,243件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Robbi!

I can boot u-boot without the error message.

The u-boot device tree should be the next:

 

&usdhc2 {
	pinctrl-names = "default", "state_100mhz", "state_200mhz";
	pinctrl-0 = <&pinctrl_usdhc2>;
	pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
	pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
	vmmc-supply = <&reg_usdhc2_vmmc>;
	bus-width = <4>;
	non-removable;
	status = "okay";
	no-sdio;
	no-mmc;
};

	pinctrl_usdhc2: usdhc2grp {
		fsl,pins = <
			MX93_PAD_SD2_CLK__USDHC2_CLK		0x1582
			MX93_PAD_SD2_CMD__USDHC2_CMD		0x40001382
			MX93_PAD_SD2_DATA0__USDHC2_DATA0	0x40001382
			MX93_PAD_SD2_DATA1__USDHC2_DATA1	0x40001382
			MX93_PAD_SD2_DATA2__USDHC2_DATA2	0x40001382
			MX93_PAD_SD2_DATA3__USDHC2_DATA3	0x40001382
			MX93_PAD_SD2_VSELECT__USDHC2_VSELECT	0x51e
		>;
	};

 

Result:

 

U-boot booting without error from SD card

Chavira_0-1747145189398.png

 

If you want to boot from SD card there is not needed the cd function since the SD should not be disconnected from the board.

 

Your custom board only has SD boot?

 

I made the next changes in Linux Kernel device tree and the card detection is working good without CD gpio configured:

&usdhc2 {
	pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep";
	pinctrl-0 = <&pinctrl_usdhc2>;
	pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
	pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
	pinctrl-3 = <&pinctrl_usdhc2_sleep>;
	broken-cd;
	fsl,cd-gpio-wakeup-disable;
	vmmc-supply = <&reg_usdhc2_vmmc>;
	bus-width = <4>;
	status = "okay";
	no-sdio;
	no-mmc;
};


	pinctrl_usdhc2: usdhc2grp {
		fsl,pins = <
			MX91_PAD_SD2_CLK__USDHC2_CLK		0x1582
			MX91_PAD_SD2_CMD__USDHC2_CMD		0x1382
			MX91_PAD_SD2_DATA0__USDHC2_DATA0	0x1382
			MX91_PAD_SD2_DATA1__USDHC2_DATA1	0x1382
			MX91_PAD_SD2_DATA2__USDHC2_DATA2	0x1382
			MX91_PAD_SD2_DATA3__USDHC2_DATA3	0x1382
			MX91_PAD_SD2_VSELECT__USDHC2_VSELECT	0x51e
		>;
	};

	pinctrl_usdhc2_100mhz: usdhc2-100mhzgrp {
		fsl,pins = <
			MX91_PAD_SD2_CLK__USDHC2_CLK		0x158e
			MX91_PAD_SD2_CMD__USDHC2_CMD		0x138e
			MX91_PAD_SD2_DATA0__USDHC2_DATA0	0x138e
			MX91_PAD_SD2_DATA1__USDHC2_DATA1	0x138e
			MX91_PAD_SD2_DATA2__USDHC2_DATA2	0x138e
			MX91_PAD_SD2_DATA3__USDHC2_DATA3	0x138e
			MX91_PAD_SD2_VSELECT__USDHC2_VSELECT	0x51e
		>;
	};

	pinctrl_usdhc2_200mhz: usdhc2-200mhzgrp {
		fsl,pins = <
			MX91_PAD_SD2_CLK__USDHC2_CLK		0x15fe
			MX91_PAD_SD2_CMD__USDHC2_CMD		0x13fe
			MX91_PAD_SD2_DATA0__USDHC2_DATA0	0x13fe
			MX91_PAD_SD2_DATA1__USDHC2_DATA1	0x13fe
			MX91_PAD_SD2_DATA2__USDHC2_DATA2	0x13fe
			MX91_PAD_SD2_DATA3__USDHC2_DATA3	0x13fe
			MX91_PAD_SD2_VSELECT__USDHC2_VSELECT	0x51e
		>;
	};

	pinctrl_usdhc2_sleep: usdhc2grpsleep {
		fsl,pins = <
			MX91_PAD_SD2_CLK__GPIO3_IO1            0x51e
			MX91_PAD_SD2_CMD__GPIO3_IO2		0x51e
			MX91_PAD_SD2_DATA0__GPIO3_IO3		0x51e
			MX91_PAD_SD2_DATA1__GPIO3_IO4		0x51e
			MX91_PAD_SD2_DATA2__GPIO3_IO5		0x51e
			MX91_PAD_SD2_DATA3__GPIO3_IO6		0x51e
			MX91_PAD_SD2_VSELECT__GPIO3_IO19	0x51e
		>;
	};

 

Result:

Booting from MMC the SD cards are detected and mounted in the system without errors

Chavira_0-1747150431296.png

 

Best Regards!

Chavira

0 件の賞賛
返信