Using CST 3.3.1 with AWS cloudHSM error with Openssl 1.1.1k

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CST 3.3.1 with AWS cloudHSM error with Openssl 1.1.1k

2,026件の閲覧回数
TheStrangeQuark
Contributor I

Hello,

I am trying to walk through the user guide for CST 3.3.1 for generating a CSF binary signature. I am doing this with keys stored on AWS cloudHSM and have openssl 1.1.1k and using PKCS#11. CloudHSM does not support adding pins to private keys, so I have the private keys in the HSM and the certificates locally. My hsm.cfg file looks like

 

# hsm stuff
hsm:
{
module = "/opt/cloudhsm/lib/libcloudhsm_pkcs11.so";
pin = "ep800_hab_test:ep800password";
slot = 0;
objects = (
{ file = "../crts/CSF1_1_sha256_secp384r1_v3_usr_crt.pem";
id = "100";
},
{ file = "../crts/IMG1_1_sha256_secp384r1_v3_usr_crt.pem";
id = "101";
});
};

After trying to compile the source code as described in the user guide, I found that I was missing libfrontend.a but was able to find it from a newer download of the source code and was able to then compile. After running the tool, I encountered a segmentation fault:

19105 Segmentation fault      (core dumped) ../code/back_end-hsm/src/cst -i csf_spl.txt -o csf_spl.bin

 

and debugged this to find that it was coming from code/back_end-hsm/src/backend.c in line 607 from the line

ENGINE_ctrl_cmd_string (eng, "MODULE_PATH", hsm_conf.module_path, 0);

 

Is there a specific version of openssl I should be using for using the code-signing tool?

I included a pdf of the user guide I was using for this.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,003件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

To search the IMX_CST_TOOL_NEW from nxp.com and refer to it. And It seems HSM backend deprecated.

 

Best regards

Harvey

0 件の賞賛
返信