Using CCM_CLK2 for RTC Clock Output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CCM_CLK2 for RTC Clock Output?

Jump to solution
2,167 Views
johnkell
Contributor I

On the i.MX6SoloX, is it possible to output the 32 kHz RTC clock on the CCM_CLK2 pin?

Thanks,

John Kell

Labels (1)
0 Kudos
Reply
1 Solution
2,062 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,062 Views
johnkell
Contributor I

Hi Igor,

Thanks for your quick response and for pointing me to the register setting for CLKO2!

Best Regards,

John

0 Kudos
Reply