Using CCM_CLK2 for RTC Clock Output?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using CCM_CLK2 for RTC Clock Output?

跳至解决方案
2,119 次查看
johnkell
Contributor I

On the i.MX6SoloX, is it possible to output the 32 kHz RTC clock on the CCM_CLK2 pin?

Thanks,

John Kell

标签 (1)
0 项奖励
回复
1 解答
2,014 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,015 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,014 次查看
johnkell
Contributor I

Hi Igor,

Thanks for your quick response and for pointing me to the register setting for CLKO2!

Best Regards,

John

0 项奖励
回复