Using CCM_CLK2 for RTC Clock Output?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CCM_CLK2 for RTC Clock Output?

ソリューションへジャンプ
2,121件の閲覧回数
johnkell
Contributor I

On the i.MX6SoloX, is it possible to output the 32 kHz RTC clock on the CCM_CLK2 pin?

Thanks,

John Kell

ラベル(1)
0 件の賞賛
返信
1 解決策
2,016件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,017件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

options for CCM_CLK2 are given in sect.19.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6SX Reference Manual and unfortunately seems there is no such option.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,016件の閲覧回数
johnkell
Contributor I

Hi Igor,

Thanks for your quick response and for pointing me to the register setting for CLKO2!

Best Regards,

John

0 件の賞賛
返信