Using ALSA on i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using ALSA on i.MX6

跳至解决方案
3,009 次查看
Kampi
Contributor I

Hi,

I tried to use ALSA in a C program with the "imx-image-full-imx6qpdlsolox" image on my i.MX6 Sabre with an example from the Internet but the compiler tells me that "#include <alsa/asoundlib.h>" is not found.

How can I add it to the system?

0 项奖励
回复
1 解答
2,938 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @Kampi!

Yes, you can install the SDK on your host using Yocto Project.

You have to compile your own SDK.

Downloading our source following the Yocto Project User Guide.

You have to compile the SDK using the next command

$ bitbake imx-image-full -c populate_sdk

And the output is a .sh, you only have to run the script and then the SDK is instaling automatically

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

Best Regards!

Chavira

在原帖中查看解决方案

3 回复数
2,963 次查看
Kampi
Contributor I

Hi,

thank you for the help. I guess I wasn´t specific enough, because I don´t need the SDK for my host. I need it for the Sabre board because I´m using VS Code for remote development. I run the command with img-image-full, because I´ve downloaded the full image from NXP.

The resulting SDK is for a x86_64 host:

$ /mnt/fsl-imx-wayland-glibc-x86_64-imx-image-full-cortexa9t2hf-neon-imx6qsabresd-toolchain-6.1-mickledore.sh
Error: Incompatible SDK installer! Your host is armv7l and this SDK was built for x86_64 hosts.

Is there a way to install the SDK on the host?

0 项奖励
回复
2,939 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @Kampi!

Yes, you can install the SDK on your host using Yocto Project.

You have to compile your own SDK.

Downloading our source following the Yocto Project User Guide.

You have to compile the SDK using the next command

$ bitbake imx-image-full -c populate_sdk

And the output is a .sh, you only have to run the script and then the SDK is instaling automatically

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

Best Regards!

Chavira

2,983 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @Kampi!

If you have extracted the toolchain from Yocto it should be correct. You can generate a .sh to install the toolchain using Yocto with the following command:

$ bitbake imx-image-multimedia -c populate_sdk

The default path for installing the toolchain is /opt, your toolchain should have the asound header on a couple of paths. If this is not available there may be a problem with the toolchain.

/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/sys/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/asoundlib.h
/opt/<DISTRO>/<BSP>/sysroots/armv8a-poky-linux/usr/include/alsa/asoundlib.h

Best Regards!

Chavira

0 项奖励
回复