Using 3.3V NAND or SD as i.MX51 boot devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using 3.3V NAND or SD as i.MX51 boot devices

814 次查看
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic: Boot Loader

 

Question.  Is it possible to use 3.3V NAND or SD devices as boot devices with i.MX51 processor?

 

Answer.  Default value of register IOMUXC_SW_PAD_CTL_PAD_NANDF_** HVE bit is 1. This means that supply voltage for NVCC_NANDF_x needs to be between 1.65-1.95V (UHVIO_L) or 2.5-3.1V(UHVIO_H).  iROM does not change this value. Applying 3.3V to NVCC_NANF_x may cause problems. If one would like to apply 3.3V to NVCC_NANDF_x, the following sequence is recommended.

 

1.When powering up i.MX51, apply 1.65-1.95 or 2.5-3.1V to NVCC_NANDF_x.

 

2.Bootloader sets HVE as 0.

 

3.Raise NVCC_NANDF_x voltage up to 3.3V.

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

标记 (1)
0 项奖励
回复
0 回复数