Use switched debug console port, the OS is hung.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use switched debug console port, the OS is hung.

跳至解决方案
5,738 次查看
charleshuang
Senior Contributor II

The default debug console is ttymxc0.

Modify console port to ttymxc1 in bootargs_base variable of uboot environmental configure, as follow:

setenv bootargs_base 'setenv bootargs console=ttymxc1,115200 enable_wait_mode=off video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'

The OS is hung after “cat /dev/ttymxc0”.

Could I switch the debug console port without modifying these code, as follow.

In uboot:

1. #define CONFIG_UART_BASE_ADDR   UART1_BASE_ADDR

2. static void setup_uart(void)

{

  /* UART1 TXD */

  mxc_iomux_v3_setup_pad(MX6Q_PAD_CSI0_DAT10__UART1_TXD);

  /* UART1 RXD */

  mxc_iomux_v3_setup_pad(MX6Q_PAD_CSI0_DAT11__UART1_RXD);

}

In Kernel:

3. uart_clk = clk_get_sys("imx-uart.0", NULL);

4. early_console_setup(UART1_BASE_ADDR, uart_clk);

标签 (2)
1 解答
5,145 次查看
justin_jiang
NXP Employee
NXP Employee

Base on my knowledge. The number of console is related to your HW UART port and kernel load sequency.

So the code midification is needed. It can't be changed just by the u-boot parameters.

在原帖中查看解决方案

13 回复数
5,145 次查看
YixingKong
Senior Contributor IV

Charles

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复
5,145 次查看
YixingKong
Senior Contributor IV

Charles

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复
5,145 次查看
charleshuang
Senior Contributor II

If it is necessary to modifying the code, what is variable "console=" used for?

It has decided the used UART port in the begin of u-boot and kernel

It seems redundant about passing "console=" to kernel

0 项奖励
回复
5,145 次查看
YixingKong
Senior Contributor IV

Charles

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复
5,145 次查看
charleshuang
Senior Contributor II

I don't think my question get really solved.

The solution Linda supplied is work, but it still need to modify code

I'd like to know if I could switch console(uart) via the setting of the variable "console=" without modifying any code.

I tried it before, I set "console=ttymxc1", but the OS is hung after“cat /dev/ttymxc0”.

So, I think ttymxc0 driver is not relly released while the setting is "console=ttymxc1"

0 项奖励
回复
5,146 次查看
justin_jiang
NXP Employee
NXP Employee

Base on my knowledge. The number of console is related to your HW UART port and kernel load sequency.

So the code midification is needed. It can't be changed just by the u-boot parameters.

5,145 次查看
YixingKong
Senior Contributor IV

Charles

I will ask one of Freescale AE to help you.

Thanks,

Yixing

0 项奖励
回复
5,145 次查看
YixingKong
Senior Contributor IV

JiangJustin, could you please help this customer?

Thanks,

Yixing

0 项奖励
回复
5,145 次查看
charleshuang
Senior Contributor II

Hi, Jimmy

So, not only uboot environment variables need to be adjusted, but also some codes for debug console port switch should be modified , is it right?

0 项奖励
回复
5,145 次查看
charleshuang
Senior Contributor II

Why can I not switch consoles by uboot environment variables?

I think consoles would be reinitialized in the kernel.

Do you have any idea about this?

0 项奖励
回复
5,139 次查看
xiaoqianlin
NXP Employee
NXP Employee

Please refer to the attached on how to customize UART port.

Regards, Linda

Linda Lin
0 项奖励
回复
5,139 次查看
jimmychan
NXP TechSupport
NXP TechSupport

right.

0 项奖励
回复
5,139 次查看
jimmychan
NXP TechSupport
NXP TechSupport

ttymxc0 is UART1

ttymxc1 is UART2

0 项奖励
回复