Hello,
The boot scenario to use the eMMC second boot partition is not supported by i.MX boot ROM,
at least, directly. Nevertheless, customers can apply the approach, described in section 6.6.5.3.5
(Redundant boot support for expansion device) of the i.MX7D RM, assuming that the secondary
bootloader, run by the boot ROM, can program properly BOOT_PARTITION_ENABLE field in the
Ext_CSD[179] and try to reboot the system. Note, "the boot partition can be selected for an MMC4.x
card after the card initialization is complete. The ROM code reads the BOOT_PARTITION_ENABLE
field in the Ext_CSD[179] to get the boot partition to be set."
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.