Use CSI interface to send data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use CSI interface to send data

1,814件の閲覧回数
1603354597
Contributor II

hi,

   I have an i.mx8mq evk with a dsi interface and a csi interface , I want to know is there any way to make csi work as dsi. Actually, I want to use CSI interface to send DSI's data.

    

   Any answer will be helpful. 

0 件の賞賛
返信
2 返答(返信)

1,749件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王 澳

unfortunately mipi-csi can be used only for data input, may be useful

to look at its documentation on:

MIPI Camera Serial Interface 2 (MIPI CSI-2) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,749件の閲覧回数
1603354597
Contributor II

Hi igo

   Thank you for your reply, by the  way, if I configure CSI as DSI  in the dts file, is that effective?

   Let me put it another way,could CSI's hardware interface be configured as DSI? I want to use two mipi panels, sadly only one DSI on the i.mx8mq evk.

   

   Best regards 

   澳刚

0 件の賞賛
返信