Use 8-bit TFT imx6ul with Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use 8-bit TFT imx6ul with Yocto

1,536 Views
jaspernuytten
Contributor I

Hi,

my guts is telling me that it's possible to connect a 8-bit interface TFT with the imx6ul but I'm not able to pin down how. Can somebody put me on the right track? I know it has something to do with the ELCDIF frame buffer driver and change some settings in the dtsi but I'm not able to find the correct documentation. Any advice/little push in the right direction?

Thanks

Labels (3)
0 Kudos
Reply
3 Replies

1,374 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jasper

please check mpu lcd patch
https://community.nxp.com/docs/DOC-331754

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,374 Views
jaspernuytten
Contributor I

Will this work on this board as well? DART-6UL - Variscite Wiki 
Or is the patch board-independent and just used as a reference?

Also, I'm using a kernel Version 4.1 and the patch is for an older version.

I also do not have the 'mxc' folder in the '/drivers/video/' folder, what can be the cause of this?

0 Kudos
Reply

1,374 Views
igorpadykov
NXP Employee
NXP Employee

patches are written and verified on nxp reference boards with nxp bsps on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

it may need porting for other boards and linux distributions.

0 Kudos
Reply