[Urgent]Max value of drain-source voltage and sink current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Urgent]Max value of drain-source voltage and sink current

Jump to solution
3,037 Views
ko-hey
Senior Contributor II

Hi all

Please tell me the max value of drain-source voltage and sink current.

My customer built their custom board with i.MX6Q and i.MX6DL and they need the spec because they have to make some document for their end customer.

In the situation, they tried to find the value of them in the datasheet such as IMX6DQIEC.

Specially, they checked "4.6.2 General Purpose I/O (GPIO) DC Parameters".

However, they can't find those values.

So could you tell me the following value ?

Q1-1

What is the max value of drain-source voltage in i.MX6Q ?

Q1-2

What is the max value of sink current in i.MX6Q ?

Q2-1

What is the max value of drain-source voltage in i.MX6DL ?

Q2-2

What is the max value of sink current in i.MX6DL ?

Ko-hey

Labels (3)
0 Kudos
Reply
1 Solution
2,789 Views
Yuri
NXP Employee
NXP Employee

OVDD is maximum.

Absolute Maximum Ratings (not operational): from -0.5   till OVDD+0.3 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
8 Replies
2,789 Views
Yuri
NXP Employee
NXP Employee

Hello,

  "The drive current is affected by the configuration of the buffer. For those buffers, you can
use to DSE field in the controlling IOMUX registers to set the drive strength. There are also
a slew rate controls in those registers which may also have an effect."

  Please refer to the following app note for more details.

“Influence of Pin Setting on System Function and Performance”

http://www.nxp.com/assets/documents/data/en/application-notes/AN5078.pdf 

   The best way to estimate currents is to use the IBIS model for the IO(s) you care about.

Please refer to i.MX6 Hardware Development Guide, Chapter 7 (Understanding the IBIS Model)

how to use parameters, provided in the model.

<
http://cache.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf  >

 IBIS file shows tables with the buffer drive current across a range of pad voltages. You can look through the
list to find the current at the voltage of interest.


"Note that the IBIS model covers a wider range than the conditions allowed in the datasheet so not everything

in the IBIS model is an allowed use case. Also, these currents in a real case would be transient lasting only

nanoseconds or less. This does not imply you could run the buffer at that current for an extended period of time.

That would cause overheating on the part and create reliability problems."

Regards,

Yuri.

0 Kudos
Reply
2,789 Views
ko-hey
Senior Contributor II

Hello Yuri

How about the max value of drain-source voltage ?

Can I find it from IBIS mode, too ?

If yes, please let me know how to find it.

I can't understand how to get drain-source voltage value from your explanation.

Ko-hey

0 Kudos
Reply
2,789 Views
Yuri
NXP Employee
NXP Employee

  As for voltages, please refer to table “General Purpose I/O (GPIO) DC Parameters” of the Datasheets.

 

~Yuri.

0 Kudos
Reply
2,789 Views
ko-hey
Senior Contributor II

Which parameter is it ?

Could you specify which I need ?

Here is the example which is from IMX6DQIEC.

image001.png

Ko-hey

0 Kudos
Reply
2,790 Views
Yuri
NXP Employee
NXP Employee

OVDD is maximum.

Absolute Maximum Ratings (not operational): from -0.5   till OVDD+0.3 

Regards,

Yuri.

0 Kudos
Reply
2,789 Views
ko-hey
Senior Contributor II

According to the Table 4 of IMX6DQIEC, the max of GPIO supply voltage is 3.6V.

So I think the max of OVDD is 3.6V.

Am I wrong ?

Ko-hey

0 Kudos
Reply
2,789 Views
Yuri
NXP Employee
NXP Employee

Hello,

 below we can find  input / output max voltage as OVDD + 0.3 

pastedImage_1.png

Also two comments may be provided :


1.

  "These are stress ratings only. Functional operation of the device at these or any other conditions beyond those
indicated in the Operating Ranges or Parameters tables is not implied."

2. 

  GPIO OVDD max = 3.6 V

Regards,

Yuri.

2,789 Views
ko-hey
Senior Contributor II

Hello Yuri

I understand the max is 3.6V.

Thank you.

Ko-hey

0 Kudos
Reply