Upgrade to Linux kernel 5.9.11 Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Upgrade to Linux kernel 5.9.11 Problem

1,612 Views
talel_hajsalem
Contributor III

Hi,

NXP until this moment has the latest release which is 5.4.47.

I'm working on some modules like SN65DSI86 and ov5647 raspberry camera and their drivers are updates in the 5.9.10 or 5.9.11 Linux kernel.

I looked into https://source.codeaurora.org/external/imx/linux-imx/ and it seems there is a tag for 5.9.11 https://source.codeaurora.org/external/imx/linux-imx/tag/?h=v5.9.11

I tried to create a recipe similar to the linux-imx_5.4.bb trying to upgrade to 5.9.11 but it failed fetching.

Can you help me with a recipe to upgrade the kernel?

Thanks, Talel

 

Labels (1)
0 Kudos
Reply
1 Reply

1,607 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Talel,

 

The L5.9.11 still on development and something may not work use the L5.4.47 instead, now if you want to downground to 4.9.11 you will have to downground the kernel as well.

 

Regards

 

0 Kudos
Reply