Updated Default Display Orientation for Android 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Updated Default Display Orientation for Android 10

3,194 次查看
tpe
Contributor III

Hello,

My aim is to change the default display orientation to portrait mode on a iMX8M device running the AndroidQ-10.0.0 release. I found an older thread that referenced a couple patches that allows the property ro.sf.hwrotation to be configured for my needs here. However, these patches no longer hold for Android 10. Are there any updates patches? If not, is there another updated way to achieve this?

Thank you,

Tony 

0 项奖励
回复
3 回复数

3,153 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tpe,

 

The latest BSP for android 10 is https://www.nxp.com/webapp/Download?colCode=Q10.0.0_2.3.0_ANDROID_SOURCE&appType=license

 

That includes the patch for display rotation, however you can add buildin SF_PRIMARY_DISPLAY_ORIENTATION=90  or  "content insert " cmd control at run time.

Regards

 

0 项奖励
回复

2,595 次查看
edward_fu
Contributor III

Hi Bio,

I have the same problem. I added SF_PRIMARY_DISPLAY_ORIENTATION=90 in BoardConfig.mk. But it seems no use. I did as this thread How-to-make-android-system-display-vertically-rotate-270-degree

0 项奖励
回复

3,081 次查看
tpe
Contributor III

Hello,

 

Thank you for your help! How do I rotate the touch input as well? Also, is there another property for secondary/multi-displays? Something like SF_SECONDARY_DISPLAY_ORIENTATION? 

 

Best regards,
Tony

0 项奖励
回复