Unused pin connection for uSDHC data pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused pin connection for uSDHC data pin

1,531 Views
ko-hey
Senior Contributor II

Hi all

I have a question about SDx_DATAx pin settings in i.MX6DL.

I plan to use SD card for boot.

SD card only use 4 bit. So I use only SDx_DATA0 to SDx_DATA3.

Does NXP have any recommendation for unsued pin connection ?

Also please let me know the register settings for unused pin.

Ko-hey

Labels (2)
0 Kudos
Reply
4 Replies

1,431 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Unused SDx_DATA[4-7] may be configured as GPIO, input, pulled up.

Note, this is default, Out of Reset state.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,431 Views
ko-hey
Senior Contributor II

Hi Yuri

Thank you for quick reply.

I understand it set as default.

How about pin connection ?

Do you recommend the pin connect to GND ? Or can I it to float ?

Ko-hey

0 Kudos
Reply

1,430 Views
Yuri
NXP Employee
NXP Employee

yes, the pins should be left floating.

~Yuri.

0 Kudos
Reply

1,431 Views
ko-hey
Senior Contributor II

Hi Yuri

Thank you for your support.

I understand.

Ko-hey

0 Kudos
Reply