Unlock RNG with cst 2.3.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unlock RNG with cst 2.3.2?

1,435件の閲覧回数
colinhelliwell
Contributor III

Could I get confirmation please about having:

[Unlock]
Engine = CAAM
Features = RNG

in the csf file. AN4581 says that this is included by default on CST v2.3+, but I've also read that it in fact is still needed (when wanting to use this one of the two options).

Just wanted to double-check please. And does it only matter if encryption is being used?

ラベル(1)
0 件の賞賛
返信
1 返信

1,307件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

 one can refer to the document as below:

https://community.nxp.com/docs/DOC-330622 

it seems you should add them to the u-boot.csf

0 件の賞賛
返信