Understanding Volume Control Mechanisms in Qt Multimedia for SGTL5000 Audio Codec

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Understanding Volume Control Mechanisms in Qt Multimedia for SGTL5000 Audio Codec

765 次查看
Niranj
Contributor I

Hello,

I have successfully integrated the SGTL5000 audio codec into an iMX6 System-on-Module (SOM). Qt Multimedia is utilized to control the codec's volume, and overall, the system functions smoothly. However, I am intrigued about the process by which Qt Multimedia alters the volume settings.

Upon monitoring the value in the codec's volume register, I've noticed that different values are written to the volume register when I adjust the volume using the amixer command (amixer sset PCM 100%). However, when I attempt to modify the volume using Qt Multimedia, the value in the volume register remains unchanged.

I am seeking clarification on how Qt Multimedia communicates with the audio codec driver to effect volume changes. Understanding this process in greater detail would greatly assist me in optimizing the integration of the audio codec into our system.

Thank you.

0 项奖励
回复
1 回复

742 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

I suggest you take a look on the next link.

 

Maybe you should consult directly with Qt

 

Best regards.

0 项奖励
回复