Unable to store keys in key ring using keyctl

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to store keys in key ring using keyctl

7,096 次查看
dpatil
Contributor II

Hi all,

I am following AN12714[latest version] for encryption storage using CAAM secure keys.

I have successfully generated keys using caam-keygen.

I successfully added a key based on the generated black key in the key retention service using "keyctl"

Following is the output:

root@imx7-var-som:/# cat /data/caam/randomkey | keyctl padd logon logkey: @s
765699361

but when I check using keyctl then same id doesn't appear

Following is output:

root@imx7-var-som:/# keyctl list @s
1 key in keyring:
24465593: --alswrv 0 65534 keyring: _uid.0

Can anyone tell me what is reason?

My kernel version is 5.4.127

and keyutils version is 1.6.1

Regards,

dpatil

 

 

 

标签 (3)
8 回复数

6,814 次查看
michael_glembot
Contributor IV

Hi @dpatil,

on 5.4.XX a session doesn't seem to be created automatically.

This should do the trick:

$ keyctl session

Another small note to @Yuri. Your answer is of poor quality.

6,408 次查看
craigmcqueenir
Contributor IV

Alternatively maybe:

keyctl new_session

That creates a new session in the current process (eg current shell) rather than in a sub-shell.

0 项奖励
回复

6,385 次查看
craigmcqueenir
Contributor IV

I found that keyctl new_session worked fine in a terminal login, but I wanted to make a kernel initramfs script to do root filesystem encryption.

I found that it failed within the context of an initramfs script, producing an error:

 

 

keyctl_session_to_parent: Operation not permitted

 

 

So far, I haven't figured out why it fails in this situation, or how to resolve it. I can create a user key for user root, rather than a session key, but I'd rather create a session key.

Looking in the keyctl_session_to_parent() function in the Linux source, it looks as though it might fail because (maybe; I haven't confirmed):

  • The initramfs script is running as PID 1 (init).
  • The parent process is PID 1 (init).
  • The initramfs script is running SUID/SGID.
0 项奖励
回复

6,381 次查看
Eximius
Contributor III

Adding it to the user session solved this problem for me. No new session necessary, just:

cat /data/caam/randomkey | keyctl padd logon logkey: @US

7,066 次查看
dpatil
Contributor II

Hi Yuri,

Thanks for your reply.

My kernel configuration related to CAAM are as follows:

# CONFIG_CRYPTO_DEV_FSL_CAAM_DMA is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_COMMON=y
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_KEYBLOB_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO=y
CONFIG_CRYPTO_DEV_FSL_CAAM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG=y
CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC_COUNT_THLD=255
CONFIG_CRYPTO_DEV_FSL_CAAM_INTC_TIME_THLD=2048
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y
# CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API_TEST is not set
# CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE=7
# CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST is not set

Please find kernel configuration in attachment let me know if anything is missing in kernel configuration

0 项奖励
回复

7,072 次查看
Yuri
NXP Employee
NXP Employee

@dpatil 
Hello,

  in the app note  NXP BSP imx-5.4.47-2.2.0 is mentioned.
What release (5.4.127) was used in Your case?

  Please check Your configuration, using  Appendix A (Configuration)
of the app note.

Regards,
Yuri.

0 项奖励
回复

7,059 次查看
dpatil
Contributor II

Hi Yuri,

Please find the attached kernel configuration.

Configurations are set as per application note

Regards,

Dhananjay Patil

0 项奖励
回复

7,013 次查看
Yuri
NXP Employee
NXP Employee

@dpatil 
Hello,

  Is it possible to use NXP Linux BSP?

Regards,
Yuri.

0 项奖励
回复