U-Boot 2014.04-08637-gaffa032 (May 11 2016 - 10:04:29)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 37 C, calibration data: 0x5ab4f27d
Reset cause: WDOG
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=11
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:2
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
booti mmc2
kernel @ 14008000 (6723120)
ramdisk @ 15000000 (497370)
fdt @ 14f00000 (50782)
kernel cmdline:
use boot.img command line:
console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 vidM
switch to ldo_bypass mode!
Using Device Tree in place at 14f00000, end 14f0f65d
Starting kernel ...
Booting Linux on physical CPU 0x0
Initializing cgroup subsys cpu
Initializing cgroup subsys cpuacct
Linux version 3.10.53-06481-g1c3a910 (b18293@scmbld4) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #4 SMP PREEMPT Thu Jan 8 14:16:27 5
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: CMA: reserved 384 MiB at 32000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @817d9000 s9728 r8192 d14848 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 259840
Kernel command line: console=ttymxc0,115200 androidboot.console=ttymxc0 consoleblank=0 vmalloc=256M init=/init video=mxcfb0:dev=hdmi,1920x1080M@M
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 959MB 64MB = 1023MB total
Memory: 627668k/627668k available, 420908k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80e51868 (14631 kB)
.init : 0x80e52000 - 0x80ea7600 ( 342 kB)
.data : 0x80ea8000 - 0x80f2b740 ( 526 kB)
.bss : 0x80f2b740 - 0x80fc02f8 ( 595 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.2
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 512
Initializing cgroup subsys debug
Initializing cgroup subsys freezer
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x807bf708 - 0x807bf760
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: Booted secondary processor
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: Booted secondary processor
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
!!request miniPCIE Power On gpio
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
pureg-dummy: no parameters
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 484K (85000000 - 85079000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx6_busfreq busfreq.16: DDR medium rate not supported.
Bus freq driver module loaded
bt power gpio is:2
mxc_bt_rfkill driver success loaded
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_ir consumer_ir.41: unable to request PWM.
platform consumer_ir.41: Driver mxc_ir requests probe deferral
console [pstore-1] enabled
ramoops: attached 0x100000@0x4bf00000, ecc: 0/0
mxc_ramoops device success loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
audit: initializing netlink socket (disabled)
type=2000 audit(0.480:1): initialized
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
NTFS driver 2.1.30 [Flags: R/W DEBUG].
jffs2: version 2.2. (NAND) �용 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 1994
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34
imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc
mxc_lcdif lcd.34: Error applying setting, reverse things back
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2084000.pwm; cannot claim for lcd.34
imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd.34) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 on device 20e0000.iomuxc
mxc_lcdif lcd.34: Error applying setting, reverse things back
mxc_lcdif lcd.34: can't get/select pinctrl
mxc_lcdif: probe of lcd.34 failed with error -22
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.30: registered mxc display driver hdmi
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 240x67
mxc_sdc_fb fb.31: Can't get fb option for mxcfb1!
mxc_sdc_fb fb.32: Can't get fb option for mxcfb2!
mxc_sdc_fb fb.33: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full lay: 1, Metal lay: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1150 mV
SW1C: 300 <--> 1875 mV at 1175 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_COL1 already requested by 21f4000.serial; cannot claim for 2008000.ecspi
imx6q-pinctrl 20e0000.iomuxc: pin-128 (2008000.ecspi) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 128 on device 20e0000.iomuxc
spi_imx 2008000.ecspi: Error applying setting, reverse things back
m25p80 spi32766.0: found mr25h256, expected m25p32
m25p80 spi32766.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
CAN device driver interface
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 3.10.53-06481-g1c3a910 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
usb 1-1: new high-speed USB device number 2 using ci_hdrc
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: EHCI Host Controller
usb usb2: Manufacturer: Linux 3.10.53-06481-g1c3a910 ehci_hcd
usb usb2: SerialNumber: ci_hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
usbcore: registered new interface driver wacom
usb 1-1: New USB device found, idVendor=05e3, idProduct=0608
usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
usb 1-1: Product: USB2.0 Hub
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
elan-touch 2-0010: elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -22
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
usb 1-1.1: new low-speed USB device number 3 using ci_hdrc
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
usb 1-1.1: New USB device found, idVendor=0461, idProduct=4e22
usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1.1: Product: USB Optical Mouse
usb 1-1.1: Manufacturer: PixArt
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
mxc_v4l2_output v4l2_out.38: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.38: V4L2 device registered as video17
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
gspca_main: v2.14.0 registered
usb 1-1.3: new high-speed USB device number 4 using ci_hdrc
mag3110 2-000e: check mag3110 chip ID
input: FreescaleMagnetometer as /devices/virtual/input/input1
input: eCompass as /devices/virtual/input/input2
mag3110 2-000e: mag3110 is probed
usb 1-1.3: New USB device found, idVendor=1618, idProduct=9113
usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=6
usb 1-1.3: Product: Wireless USB Network Module
usb 1-1.3: Manufacturer: Redpine Signals, Inc.
usb 1-1.3: SerialNumber: 000000000001
input: FreescaleAccelerometer as /devices/virtual/input/input3
mma8x5x device driver probe successfully
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
usb 1-1.4: new low-speed USB device number 5 using ci_hdrc
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.24.0-ioctl (2013-01-15) initialised: dm-devel@redhat.com
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver btusb
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
usb 1-1.4: New USB device found, idVendor=413c, idProduct=2107
usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1.4: Product: Dell USB Entry Keyboard
usb 1-1.4: Manufacturer: DELL
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
Galcore version 5.0.11.25762
mmc2: new high speed SDHC card at address e624
mmcblk2: mmc2:e624 SU08G 7.40 GiB
mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4
mmcblk2: p4 size 13352010 extends beyond EOD, truncated
mmc3: new high speed DDR MMC card at address 0001
mmcblk3: mmc3:0001 SEM08G 7.39 GiB
mmcblk3boot0: mmc3:0001 SEM08G partition 1 1.00 MiB
mmcblk3boot1: mmc3:0001 SEM08G partition 2 1.00 MiB
mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB
mmcblk3: p1 p2 p3 < p5 p6 p7 p8 p9 > p4
mmcblk3: p4 size 13303808 extends beyond EOD, truncated
mmcblk3boot1: unknown partition table
mmcblk3boot0: unknown partition table
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
hidraw: raw HID events driver (C) Jiri Kosina
input: PixArt USB Optical Mouse as /devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.1/1-1.1:1.0/input/input4
hid-generic 0003:0461:4E22.0001: input,hidraw0: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.0-1.1/input0
input: DELL Dell USB Entry Keyboard as /devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.4/1-1.4:1.0/input/input5
hid-generic 0003:413C:2107.0002: input,hidraw1: USB HID v1.11 Keyboard [DELL Dell USB Entry Keyboard] on usb-ci_hdrc.0-1.4/input0
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
wm8962 0-001a: customer id 0 revision D
input: WM8962 Beep Generator as /devices/soc0/soc.1/2100000.aips-bus/21a0000.i2c/i2c-0/0-001a/input/input6
imx-wm8962 sound.28: wm8962 <-> 202c000.ssi mapping ok
imx-audio-hdmi sound-hdmi.29: hdmi-hifi <-> hdmi_audio.17 mapping ok
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (15958 buckets, 63832 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN1: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
regulator-dummy: disabling
imx mcc test is registered.
file system registered
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
android_usb gadget: android_usb ready
input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input7
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
ALSA device list:
#0: wm8962-audio
#1: imx-hdmi-soc
Freeing unused kernel memory: 340K (80e52000 - 80ea7000)
SELinux: Permission attach_queue in class tun_socket not defined in policy.
SELinux: the above unknown classes and permissions will be denied
type=1403 audit(1.750:2): policy loaded auid=4294967295 ses=4294967295
SELinux: Loaded policy from /sepolicy
type=1404 audit(1.760:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init: /dev/hw_random not found
keychord: using input dev DELL Dell USB Entry Keyboard for fevent
keychord: using input dev gpio-keys.27 for fevent
init: cannot open '/initlogo.rle'
Console: switching to colour dummy device 80x30
EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)
EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): warning: maximal mount count reached, running e2fsck is recommended
EXT4-fs (mmcblk2p4): recovery complete
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p6): warning: maximal mount count reached, running e2fsck is recommended
EXT4-fs (mmcblk2p6): recovery complete
EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
init: /dev/hw_random not found
rfkill: BT RF going to : off
type=1400 audit��IةT�Q]�T�_�]���M�n�healthd: BatteryTemperaturePath not found
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
healthd: BatteryTechnologyPath not found
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'
init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'
init: powerctl: cannot expand '${sys.powerctl}'
init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'
init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'
android_usb: already disabled
mtp_bind_config
binder: 153:153 transaction failed 29189, size 0-0
root@sabresd_6dq:/ # ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
warning: `zygote' uses 32-bit capabilities (legacy support in use)
period 1975891114 ,timeout is -66172562, wake up is :0
period 1975891114 ,timeout is -66172562, wake up is :0
request_suspend_state: wakeup (3->0) at 22682548668 (1970-01-02 00:00:04.484456000 UTC)
period 66 ,timeout is 0, wake up is :0
mma enable setting active
lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:
lowmemorykiller: oom_adj 0 => oom_score_adj 0
lowmemorykiller: oom_adj 1 => oom_score_adj 58
lowmemorykiller: oom_adj 2 => oom_score_adj 117
lowmemorykiller: oom_adj 3 => oom_score_adj 176
lowmemorykiller: oom_adj 9 => oom_score_adj 529
lowmemorykiller: oom_adj 15 => oom_score_adj 1000
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
acc_open
acc_release
onebox_wlan_nongpl: module license 'unspecified' taints kernel.
Disabling lock debugging due to kernel taint
usbcore: registered new interface driver Onebox-USB
init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
libphy: 2188000.ethernet:01 - Link is Up - 100/Full
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Unable to register the devicewlan0
ERROR: Failed to create vap_interface
VAP = NULL
request_suspend_state: sleep (0->3) at 37991512670 (2016-05-19 08:58:00.152605667 UTC)
active wake lock PowerManagerService.Broadcasts
active wake lock PowerManagerService.WakeLocks
mma enable setting inactive
root@sabresd_6dq:/ # busyUnable to register the devicewlan0
ERROR: Failed to create vap_interface
VAP = NULL
root@sabresd_6dq:/ # netcfg
rpine0 DOWN 0.0.0.0/0 0x00001802 00:23:a7:5c:53:10
wlan0 DOWN 0.0.0.0/0 0x00001002 00:23:a7:5c:53:10
eth0 UP 192.168.3.107/24 0x00001043 00:04:9f:03:cd:f9
lo UP 127.0.0.1/8 0x00000049 00:00:00:00:00:00
root@sabresd_6dq:/ # logcat | grep Wifi
I/AudioFlinger( 163): loadHwModule() Loaded r_submix audio interface from Wifi Display audio HAL (audio) handle 4
D/WifiMonitor( 462): Creating WifiMonitor
D/WifiMonitor( 462): WifiMonitorSingleton gotten
D/WifiMonitor( 462): WifiMonitorSingleton created
D/WifiMonitor( 462): registerInterface(p2p0+android.net.wifi.p2p.WifiP2pService$P2pStateMachine@2ca00990)
E/WifiStateMachine( 462): RPS WiFi state machine starting with interface name as wlan0andwlan0
D/WifiMonitor( 462): Creating WifiMonitor
D/WifiMonitor( 462): WifiMonitorSingleton gotten
D/WifiMonitor( 462): registerInterface(wlan0+android.net.wifi.WifiStateMachine@2ca0ffa0)
D/WifiStateMachine( 462): completeConstruction: E
D/WifiStateMachine( 462): completeConstruction: maxDepth=6
D/WifiStateMachine( 462): setupInitialStateStack: E mInitialState=InitialState
D/WifiStateMachine( 462): moveTempStackToStateStack: i=1,j=0
D/WifiStateMachine( 462): moveTempStackToStateStack: i=0,j=1
D/WifiStateMachine( 462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=0,Top=InitialState
D/WifiStateMachine( 462): completeConstruction: X
D/WifiStateMachine( 462): handleMessage: E msg.what=-2
D/WifiStateMachine( 462): invokeEnterMethods: DefaultState
D/WifiStateMachine( 462): invokeEnterMethods: InitialState
D/WifiController( 462): isAirplaneModeOn = false, isWifiEnabled = true, isScanningAvailable = false
E/WifiHW ( 462): Mutyam**** Disabling protocol
E/WifiHW ( 462):
I/WifiService( 462): WifiService starting up with Wi-Fi enabled
D/WifiService( 462): setWifiEnabled: true pid=462, uid=1000
D/WifiController( 462): WifiController msg { when=0 what=155656 target=com.android.internal.util.StateMachine$SmHandler } deferred for 213ms
D/WifiController( 462): DEFERRED_TOGGLE handled
D/WifiStateMachine( 462): setting operational mode to 1
E/WifiApConfigStore( 462): Bad version on hotspot configuration file, set defaults
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131154
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131084
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131085
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131146
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131083
D/WifiStateMachine( 462): processMsg: InitialState
E/WifiHW ( 462): Loading WiFi driver here
E/WifiHW ( 462): *****common_gpl.ko inserted
E/WifiHW ( 462): *****wlan.ko inserted
E/WifiHW ( 462): ****wlan_wep.ko inserted
E/WifiHW ( 462): *****wlan_tkip.ko inserted
E/WifiHW ( 462): *****wlan_ccmp.ko inserted
E/WifiHW ( 462): ********wlan_acl.ko inserted
E/WifiHW ( 462): *****wlan_xauth.ko inserted
E/WifiHW ( 462): ***wlan_scan_sta.ko inserted
E/WifiHW ( 462): ***onebox_wlan_nongpl.ko inserted
E/WifiHW ( 462): ***onebox_wlan_gpl.ko inserted
E/WifiHW ( 462): ***onebox_bt_nongpl.ko inserted
E/WifiHW ( 462): ***onebox_bt_gpl.ko inserted
E/WifiHW ( 462): *****onebox_nongpl.ko inserted
E/WifiHW ( 462): ***********onebox_gpl.ko
E/WifiHW ( 462): ********* ALL ko inserted successfully
E/WifiHW ( 157): Mutyam****protocol enable
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Vap Creation Output:
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Inside STA wifi.c wifi_get_fw_path out_iface is wlan0
E/WifiHW ( 157): Mutyam****protocol enable
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Vap Creation Output:
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Inside AP wifi.c wifi_get_fw_path out_iface is wlan0
D/WifiMonitor( 462): WifiMonitorSingleton gotten
D/WifiStateMachine( 462): setWifiState: enabling
D/WifiStateMachine( 462): Supplicant start successful
D/WifiMonitor( 462): WifiMonitorSingleton gotten
D/WifiMonitor( 462): startMonitoring(wlan0) with mConnected = false
D/WifiMonitor( 462): connecting to supplicant
E/WifiHW ( 462): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": Permission denied
E/WifiHW ( 462): Supplicant not running, cannot connect
E/WifiHW ( 462): Supplicant not running, cannot connect
E/WifiHW ( 462): Supplicant not running, cannot connect
E/WifiHW ( 462): Supplicant not running, cannot connect
E/WifiHW ( 462): Supplicant not running, cannot connect
E/WifiMonitor( 462): startMonitoring(wlan0) failed!
D/WifiStateMachine( 462): transitionTo: destState=SupplicantStartingState
D/WifiStateMachine( 462): handleMessage: new destination call exit/enter
D/WifiStateMachine( 462): setupTempStateStackWithStatesToEnter: X mTempStateStackCount=1,curStateInfo: state=DefaultState,active=true,parent=nul
D/WifiStateMachine( 462): invokeExitMethods: InitialState
D/WifiStateMachine( 462): moveTempStackToStateStack: i=0,j=1
D/WifiStateMachine( 462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=1,Top=SupplicantStartingState
D/WifiStateMachine( 462): invokeEnterMethods: SupplicantStartingState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131144
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): deferMessage: msg=131144
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131085
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): deferMessage: msg=131085
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131149
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): setSuspendOptimizations: 2 true
D/WifiStateMachine( 462): mSuspendOptNeedsDisabled 0
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=69632
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131101
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131101
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131206
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=147458
D/WifiStateMachine( 462): processMsg: SupplicantStartingState
E/WifiStateMachine( 462): Failed to setup control channel, restart supplicant
D/WifiMonitor( 462): WifiMonitorSingleton gotten
D/WifiStateMachine( 462): transitionTo: destState=InitialState
D/WifiStateMachine( 462): handleMessage: new destination call exit/enter
D/WifiStateMachine( 462): setupTempStateStackWithStatesToEnter: X mTempStateStackCount=1,curStateInfo: state=DefaultState,active=true,parent=nul
D/WifiStateMachine( 462): invokeExitMethods: SupplicantStartingState
D/WifiStateMachine( 462): moveTempStackToStateStack: i=0,j=1
D/WifiStateMachine( 462): moveTempStackToStateStack: X mStateStackTop=1,startingIndex=1,Top=InitialState
D/WifiStateMachine( 462): invokeEnterMethods: InitialState
E/WifiHW ( 462): Mutyam**** Disabling protocol
E/WifiHW ( 462):
D/WifiStateMachine( 462): moveDeferredMessageAtFrontOfQueue; what=131085
D/WifiStateMachine( 462): moveDeferredMessageAtFrontOfQueue; what=131144
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131144
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131085
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleScreenStateChanged: true
D/WifiStateMachine( 462): handleMessage: E msg.what=131154
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131127
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131158
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): setSuspendOptimizations: 4 false
D/WifiStateMachine( 462): mSuspendOptNeedsDisabled 4
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleScreenStateChanged: false
D/WifiStateMachine( 462): handleMessage: E msg.what=131154
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131158
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): setSuspendOptimizations: 4 true
D/WifiStateMachine( 462): mSuspendOptNeedsDisabled 0
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131083
D/WifiStateMachine( 462): processMsg: InitialState
E/WifiHW ( 157): Mutyam****protocol enable
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Vap Creation Output:
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Inside STA wifi.c wifi_get_fw_path out_iface is wlan0
E/WifiHW ( 157): Mutyam****protocol enable
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Vap Creation Output:
E/WifiHW ( 157):
E/WifiHW ( 157): RAVI:****Inside AP wifi.c wifi_get_fw_path out_iface is wlan0
D/WifiMonitor( 462): WifiMonitorSingleton gotten
E/WifiStateMachine( 462): Failed to start supplicant!
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131101
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
D/WifiStateMachine( 462): handleMessage: E msg.what=131101
D/WifiStateMachine( 462): processMsg: InitialState
D/WifiStateMachine( 462): processMsg: DefaultState
D/WifiStateMachine( 462): handleMessage: X
^C
130|root@sabresd_6dq:/ # logcat | grep wpa_
E/WifiHW ( 462): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": Permission denied
I/wpa_supplicant( 914): Successfully initialized wpa_supplicant
E/wpa_supplicant( 914): wlan0: Unsupported driver 'nl80211'
I/wpa_supplicant( 1051): Successfully initialized wpa_supplicant
E/wpa_supplicant( 1051): wlan0: Unsupported driver 'nl80211'
Here i am facing issue with unable to open connection to supplicant on /data/system/wpa_supplicant/wlan0.Actually there is no wlan0 file in this /data/system/wpa_supplicant/ directory.
Que1:
How it ( "wlan0" ) will create in /data/syatem/wpa_supplicant/ directory ? For this problem i have changed all possible permissions in init.rc file.
By default wlan0 will create or we have to create ?..if we have create means,.please tell me the steps to do???
If wlan0 is created in /data/system/wpa_supplicant/,we establish connection to supplicant.So this error i need to fix first.
Que2:
And For Unsupported driver "nl80211", i compiled wpa_supplicant using bsd interface but its taking nl80211 ?..
i have enabled CONFIG_DRIVER_BSD=y in all files(defconfig,android.config,wpa_cli.c,...etc).Eventhough i am getting Unsupported driver error.
Last two weeks i am facing this problem.please anyone give solution for this issue.
Any Solutions.......!!!!
Original Attachment has been moved to: logs.zip
Solved! Go to Solution.
 
					
				
		
 weidong_sun
		
			weidong_sun
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Raj,
Refer to the link, please!
Porting BCM4330/BCM43362 WIFI to Android4.2.2
Maybe the version of BSP is not different from yours, but it can still provide some help for your porting.
Q1:
wlan0 is created by your wifi driver. you don't need to modify it.
Q2:
when you configuring linux kernel by typing " make menuconfig ", I think you should have selected "nl80211" , the issue should be generated by "Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": ".
In addition, the directory "/data/system/wpa_supplicant/wlan0" is given in wifi.c file and Boardconfig.mk file, check them , please!
Regards,
Weidong
 
					
				
		
 weidong_sun
		
			weidong_sun
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Raj,
Refer to the link, please!
Porting BCM4330/BCM43362 WIFI to Android4.2.2
Maybe the version of BSP is not different from yours, but it can still provide some help for your porting.
Q1:
wlan0 is created by your wifi driver. you don't need to modify it.
Q2:
when you configuring linux kernel by typing " make menuconfig ", I think you should have selected "nl80211" , the issue should be generated by "Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": ".
In addition, the directory "/data/system/wpa_supplicant/wlan0" is given in wifi.c file and Boardconfig.mk file, check them , please!
Regards,
Weidong
Hi Weidong,
Thanks Weidong. We cleared that error instead of passing '/data/system/wpa_supplicant/wlan0',we just gave wlan0. Now we were able to see in GUI ( Searching for Wi-Fi networks...) and Wifi enabled.
Regards,
Raj.