Unable to invert display via xrandr

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to invert display via xrandr

1,410 次查看
sheraz_ali
Contributor II

Hi,

I am trying to invert the display via xrandr 

root@PRGLT:~# export DISPLAY=:0.0
root@PRGLT:~# xrandr -q
xrandr: Failed to get size of gamma for output default
Screen 0: minimum 1024 x 600, current 1024 x 600, maximum 1024 x 600
default connected 1024x600+0+0 0mm x 0mm
1024x600 0.00*
root@PRGLT:~#

Okay, I was trying to invert my LCD using xrandr, but i am following error

root@PRGLT:~# xrandr -o inverted
X Error of failed request: BadMatch (invalid parameter attributes)
Major opcode of failed request: 139 (RANDR)
Minor opcode of failed request: 2 (RRSetScreenConfig)
Serial number of failed request: 14
Current serial number in output stream: 14
root@PRGLT:~#

Xorg Configuration File

cat /usr/share/X11/xorg.conf.d/99-fbdev.conf
Section "InputDevice"
Identifier "touchscreen"
Driver "evdev"
Option "Device" "/dev/input/event0"
EndSection

Section "Device"
Identifier "myfb"
Driver "fbdev"
Option "fbdev" "/dev/fb0"
Option "ShadowFB" "true"
Option "Rotate" "CW"
Option "RandRRotation" "on"
EndSection

Section "Screen"
Identifier "Screen0"
Device "myfb"
Monitor "Monitor0"
Option "Rotate" "CW"
SubSection "Display"
EndSubSection
EndSection

Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection

 Let me know if any configuration file needs to be changed

0 项奖励
回复
1 回复

1,407 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sheraz,

The maximum resolution is 1024x600 to invert, other solution could be rotation of the screen (180 degree) as the U-boot argument.

I added "rotation" argument handling in the drivers/video/mxc/mxc_ipuv3_fb.c, but found this code:

for the MX6Q

     if (var->rotate > IPU_ROTATE_VERT_FLIP)

                 var->rotate = IPU_ROTATE_NONE;

 

Regards

0 项奖励
回复