Unable to invert display via xrandr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to invert display via xrandr

1,427 Views
sheraz_ali
Contributor II

Hi,

I am trying to invert the display via xrandr 

root@PRGLT:~# export DISPLAY=:0.0
root@PRGLT:~# xrandr -q
xrandr: Failed to get size of gamma for output default
Screen 0: minimum 1024 x 600, current 1024 x 600, maximum 1024 x 600
default connected 1024x600+0+0 0mm x 0mm
1024x600 0.00*
root@PRGLT:~#

Okay, I was trying to invert my LCD using xrandr, but i am following error

root@PRGLT:~# xrandr -o inverted
X Error of failed request: BadMatch (invalid parameter attributes)
Major opcode of failed request: 139 (RANDR)
Minor opcode of failed request: 2 (RRSetScreenConfig)
Serial number of failed request: 14
Current serial number in output stream: 14
root@PRGLT:~#

Xorg Configuration File

cat /usr/share/X11/xorg.conf.d/99-fbdev.conf
Section "InputDevice"
Identifier "touchscreen"
Driver "evdev"
Option "Device" "/dev/input/event0"
EndSection

Section "Device"
Identifier "myfb"
Driver "fbdev"
Option "fbdev" "/dev/fb0"
Option "ShadowFB" "true"
Option "Rotate" "CW"
Option "RandRRotation" "on"
EndSection

Section "Screen"
Identifier "Screen0"
Device "myfb"
Monitor "Monitor0"
Option "Rotate" "CW"
SubSection "Display"
EndSubSection
EndSection

Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection

 Let me know if any configuration file needs to be changed

0 Kudos
Reply
1 Reply

1,424 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sheraz,

The maximum resolution is 1024x600 to invert, other solution could be rotation of the screen (180 degree) as the U-boot argument.

I added "rotation" argument handling in the drivers/video/mxc/mxc_ipuv3_fb.c, but found this code:

for the MX6Q

     if (var->rotate > IPU_ROTATE_VERT_FLIP)

                 var->rotate = IPU_ROTATE_NONE;

 

Regards

0 Kudos
Reply