Unable to get the metdata information using gplay after using ‘>’: Play the next multimedia file.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to get the metdata information using gplay after using ‘>’: Play the next multimedia file.

ソリューションへジャンプ
2,106件の閲覧回数
srinivasanshanm
Contributor III

Dear I.MX Community,

 

 

I am using L2.6.35_1.1.0_130130_source on I>MX28 BSP,

 

I am unable to get the metadata information of the next multimedia file after  giving ‘>’: Play the next multimedia file.

 

Could you please help me out in how to resolve this issue, as am unable to get the metadata information of the next multimedia file getting played, I hereby attached the log for your information,

 

Kindly do the needful as early as possible, as am stuck with this issue from many days,

 

Many Thanks in advance

Original Attachment has been moved to: logs.txt.zip

ラベル(2)
0 件の賞賛
返信
1 解決策
2,003件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I upload a patch which can fix this issue, pls use it and give me the response.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,004件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I upload a patch which can fix this issue, pls use it and give me the response.

0 件の賞賛
返信
2,003件の閲覧回数
GraceH
Senior Contributor II

I can reproduce the problem and CT 44525538 is created.

Grace

0 件の賞賛
返信