Unable to get ethernet working on kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to get ethernet working on kernel

ソリューションへジャンプ
3,672件の閲覧回数
jemish_1990
Contributor V

Hi All,

We have customized board based on iMX6Q. In which we are using Marvell switch mv88e6176. In this switch port0 is connected with external ethernet, port 6 is connected with FEC controller of IMX6Q processor, port5 is connected with MAC of other board.

We got ethernet working on u-boot level and tftp is also working. But at kernel level we got below error while booting. "IP-Config: Failed to open eth0" and  "IP-Config: No network devices available".

Initially it was failing because no PHY device. Then we make few changes related to fix phy our kernel. Now we are stuck at this stage. Any help or suggestion related to this issue will appreciated.

Thanks,

Jemish

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
3,321件の閲覧回数
bpe
NXP Employee
NXP Employee

Based on the attached boot log, the kernel does not see a valid Ethernet to configure. Besides that, I see some output in the kernel

log that suggests that you modified the driver. In general, adding a fixed-link property to the controller device tree node should

be sufficient to bypass the PHY initialization and setup the controller parameters properly without reading the PHY.

Suggestions:

1. Revert to the original BSP kernel.

2. Make sure the device tree correctly reflects the MAC/PHY interface type.

3. Use a sufficiently compact root filesystem image to TFTP it with subsequent ramboot to allow the system to complete booting.

4. Use ifconfig and ethtool to check the status of the interface

5. Use a debugger to verify that the following piece of code in fec_main.c is reached and  of_phy_register_fixed_link() is invoked.


if (!phy_node && of_phy_is_fixed_link(np)) {

    ret = of_phy_register_fixed_link(np);

        if (ret < 0) {

            dev_err(&pdev->dev,

                "broken fixed-link specification\n");

            goto failed_phy;

        }

        phy_node = of_node_get(np);

    }


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,321件の閲覧回数
bpe
NXP Employee
NXP Employee

Please share the following materials:

1. Full system boot log.

2. Your Device Tree source.

3. Output of `ifconfig -a'

Platon

0 件の賞賛
返信
3,320件の閲覧回数
jemish_1990
Contributor V

Hi Platon

Thanks for your prompt response!

Please find attached all the files as required.

I have upload full dts source code in which we are using "imx6q-lu600board.dtb"

For this .dtb file relevant files are as below:

  • imx6q-lu600board.dtb
  • imx6q-lu600board.dts
  • imx6qdl-lu600board.dtsi
  • imx6q.dtsi
  • imx6qdl-lu600board.dtsi
  • imx6qdl.dtsi
  • imx6q-pinfunc.h

Note: I am not able to boot board till the filesystem prompt so Output of "ifconfig -a" is not possible.

Let me know if anything is required.

Thanks,

Jemish !

0 件の賞賛
返信
3,322件の閲覧回数
bpe
NXP Employee
NXP Employee

Based on the attached boot log, the kernel does not see a valid Ethernet to configure. Besides that, I see some output in the kernel

log that suggests that you modified the driver. In general, adding a fixed-link property to the controller device tree node should

be sufficient to bypass the PHY initialization and setup the controller parameters properly without reading the PHY.

Suggestions:

1. Revert to the original BSP kernel.

2. Make sure the device tree correctly reflects the MAC/PHY interface type.

3. Use a sufficiently compact root filesystem image to TFTP it with subsequent ramboot to allow the system to complete booting.

4. Use ifconfig and ethtool to check the status of the interface

5. Use a debugger to verify that the following piece of code in fec_main.c is reached and  of_phy_register_fixed_link() is invoked.


if (!phy_node && of_phy_is_fixed_link(np)) {

    ret = of_phy_register_fixed_link(np);

        if (ret < 0) {

            dev_err(&pdev->dev,

                "broken fixed-link specification\n");

            goto failed_phy;

        }

        phy_node = of_node_get(np);

    }


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,320件の閲覧回数
jemish_1990
Contributor V

Hi Platon,

Thanks a lot for your value able suggestions. After going to through few links and applying below patch for fixed-link I am able to get it working now.

We can close this this discussion.

[RFC PATCHv2 2/4] net: phy: extend fixed driver with fixed_phy_register()

Thanks,

Jemish 

0 件の賞賛
返信