Dear Sir/Madam,
Can any one tested attached HDMI to VGA supported module with IMx6 Sbresd board with 3.0.35 kernel or other. If so any can help me out to interface this to the sabre board. Your inputs are highly appreciated.
Thanks & Regards,
Narasimhulu.O
Hi Narasimhulu
seems it can be connected to hdmi port of processor as usual hdmi
panel. However specs of this device are needed for providing more detailed answer.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Igor,
Thanks for reply actually i have an converter module of HDMI to VGA which is connecting from sabredsd imx6 board to dell desktop monitor VGA. But am not able to display anything on monitor.
Thanks & Regards,
Narasimhulu
Hi Narasimhulu
you should check datasheet of this device for its resolution,
then use appropriate kernel boot parameter like
video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
Best regards
igor
Hi Igor,
I am passing resolution on my bootloader is hdmi_res=1280x1024M@60. The below is kernel log.
mxc_hdmi mxc_hdmi: Read EDID again
mxc_hdmi mxc_hdmi: No modes read from edid
mxc_hdmi mxc_hdmi: create default modelist
fbcvt: 1280x1024@60: CVT Name - 1.310M4
imx-ipuv3 imx-ipuv3.0: WARNING: adapt panel end blank lines
root@SabreSD-iMX6:~ echo 1 > /sys/class/graphics/fb0/blank
root@SabreSD-iMX6:~ echo 1 > /sys/class/graphics/fb1/blank
root@SabreSD-iMX6:~ mxc_hdmi mxc_hdmi: Read EDID again
mxc_hdmi mxc_hdmi: No modes read from edid
mxc_hdmi mxc_hdmi: create default modelist
Best Regards,
Narasimha
Hi Narasimhulu
one can try the fbset command, like
fbset -fb /dev/fb0 -xres 1440 -yres 540
Best regards
igor
Hi Igor,
Thanks for the reply. Is there any module which already has tested HDMI to VGA converters before with sabreSD. If so you can suggest accordingly.
Thanks & Regards,
Narasimha
Hi Narasimhulu
unfortunately I am not aware of such modules
Best regards
igor
Hi Igor,
Here i found the datasheet for the module HDMI to VGA. Inside the module having CH7101B chip module. Please find the given link for datasheet.
http://www.chrontel.com/media/Datasheets/CH7101B%20Brief%20Datasheet%20Rev1.0.pdf
Thanks & Regards,
Narasimha
Hi Narasimhulu
suggest to check with standard hdmi panel, if it works
then this device should work too. If not, one can post issue on
Plugable Launches the HDMI to VGA Adapter Cable | Plugable
Best regards
igor
Hello Igor,
Can you please check the data-sheet once and can guide where exactly am unable to display using this module on vga display. Is there any hardware compatibility or property to support this kind of external modules to the Imx6 processor. Can you please clear these queries.
Can please give any solution for above points to clear understanding.
Thanks & Regards,
Narasimha
Hi Narasimhulu,
It is impossible to give you details based on the spec you send. electrical characteristics are here key.
It may not work just because your HDMI to VGA converter does not match the electrical specs (current).
So please measure the 5V on the HDMI side as it supplies the converter.
br,
Rod
Hello Igor,
Can you please check the data-sheet once and can guide where exactly am unable to display using this module on vga display. Is there any hardware compatibility or property to support this kind of external modules to the Imx6 processor. Can you please clear these queries.
Thanks & Regards,
Narasimha
Hello Igor,
Thank you very much for sharing the information.
Thanks & Regards,
Narasimha
Hello Igor,
Can you please check the data-sheet once and can guide where exactly am unable to display using this module on vga display. Is there any hardware compatibility or property to support this kind of external modules to the Imx6 processor. Can you please clear these queries.
Thanks & Regards,
Narasimha
Hi Igor,
Waiting for you valuable reply.
Best Regards,
Narasimha
Hi Igor,
Thanks for the reply. But what is the below logs will giving the information, anything is wrong in this case. Where exactly can trace for this, as the module is plug and play and there is no any technical datasheet for this module. I am using Barebox bootloader. If you can provide the any solution it will very useful to me.
mxc_hdmi mxc_hdmi: Read EDID again
mxc_hdmi mxc_hdmi: No modes read from edid
mxc_hdmi mxc_hdmi: create default modelist
fbcvt: Aspect ratio not CVT standard
fbcvt: 1360x768@60: CVT Name - Not a CVT standard - 1.044 Mega Pixel Image
Thanks & Regards,
Narasimha