Unable to get an image using imxeglvivsink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to get an image using imxeglvivsink

1,443 Views
anthony3
Contributor II

Using,

gst-launch-1.0 autovideosink ! imxeglvivsink

results in

Setting pipeline to PAUSED ...
ERROR: Pipeline doesn't want to pause.
Setting pipeline to NULL ...
Freeing pipeline ...

This seems to only occur when using imxeglvivsink. Does anyone know why that is?

Thanks,

Labels (2)
0 Kudos
Reply
1 Reply

1,257 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anthony

one can post issue on

Issues · Freescale/gstreamer-imx · GitHub 

Alternatively one can try nxp gstreamer plugins (imx-gst1.0-plugin)

described in Linux Guide Multimedia section in Linux L4.14.98_2.0.0 Documentation

Demo Images can be found on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply