Unable to establish SSL connection.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to establish SSL connection.

Jump to solution
7,069 Views
Mihan
Contributor IV

Hi all

I found an error when bitbake the image in VMWare-Ubuntu 18.04 with NAT mode network.

WARNING: imx-gpu-viv-1_6.4.3.p2.0-aarch32-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p2.0-aarch32.bin;fsl-eula=true, attempting MIRRORS if available
ERROR: imx-gpu-viv-1_6.4.3.p2.0-aarch32-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1551"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/vmuser/imx-yocto-bsp/sources/poky/scripts:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot/usr/bin/crossscripts:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot-native/usr/sbin:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot-native/usr/bin:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot-native/sbin:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/recipe-sysroot-native/bin:/home/vmuser/imx-yocto-bsp/sources/poky/bitbake/bin:/home/vmuser/imx-yocto-bsp/build-xwayland/tmp/hosttools"; export HOME="/home/vmuser"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/vmuser/imx-yocto-bsp/downloads/ 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p2.0-aarch32.bin' --progress=dot -v failed with exit code 4, output:
--2021-07-16 01:18:17--  https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p2.0-aarch32.bin
Resolving www.nxp.com (www.nxp.com)... 118.215.15.37
Connecting to www.nxp.com (www.nxp.com)|118.215.15.37|:443... connected.
Unable to establish SSL connection.

ERROR: imx-gpu-viv-1_6.4.3.p2.0-aarch32-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p2.0-aarch32.bin;fsl-eula=true'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/vmuser/imx-yocto-bsp/build-xwayland/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/imx-gpu-viv/1_6.4.3.p2.0-aarch32-r0/temp/log.do_fetch.50027
ERROR: Task (/home/vmuser/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-graphics/imx-gpu-viv/imx-gpu-viv_6.4.3.p2.0-aarch32.bb:do_fetch) failed with exit code '1'

 So I try opening the URL, it works well and the binary file could be downloaded.

What should I do next

 

Best regards

Mihan

0 Kudos
Reply
1 Solution
7,062 Views
Mihan
Contributor IV

Hi again

the error may be solved after I reboot the terminal. Maybe network or configure was changed.

View solution in original post

0 Kudos
Reply
3 Replies
7,057 Views
b36401
NXP Employee
NXP Employee

Please check firewall settings of your network.

0 Kudos
Reply
7,063 Views
Mihan
Contributor IV

Hi again

the error may be solved after I reboot the terminal. Maybe network or configure was changed.

0 Kudos
Reply
7,056 Views
b36401
NXP Employee
NXP Employee

Thanx for letting know. I'm glad that it was solved easily.

0 Kudos
Reply