Unable to connect with AP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to connect with AP?

1,315件の閲覧回数
vinothpenati
Contributor I

Hi all,

   I am working on wifi porting in Marshmallow BSP[6.0.1.2.1.0] in imx6sl evk. In open mode my evb is able to connect with third party AP but unable to get ip address where as other third party devices are able to connect with that AP, and similarly in AP security mode other devices are unable to connect with my AP where as in open AP mode able to connect.

Please tell me the solution to avoid this error.

Thanks,

Vinoth P B

ラベル(3)
0 件の賞賛
返信
1 返信

1,175件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinoth

please check

wifi binding on imx6sl evk based board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信