Unable to connect with AP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to connect with AP?

928 次查看
vinothpenati
Contributor I

Hi all,

   I am working on wifi porting in Marshmallow BSP[6.0.1.2.1.0] in imx6sl evk. In open mode my evb is able to connect with third party AP but unable to get ip address where as other third party devices are able to connect with that AP, and similarly in AP security mode other devices are unable to connect with my AP where as in open AP mode able to connect.

Please tell me the solution to avoid this error.

Thanks,

Vinoth P B

标签 (3)
0 项奖励
回复
1 回复

788 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinoth

please check

wifi binding on imx6sl evk based board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复