Unable to clone kernel_imx from git clone git://git.freescale.com/imx/linux-imx.git

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to clone kernel_imx from git clone git://git.freescale.com/imx/linux-imx.git

3,683件の閲覧回数
engineer_bsp01
Contributor III

Hi All,

I am trying to clone kernel-imx and uboot for android 7.1.2 but it is showing like this

Cloning into 'uboot-imx'...
fatal: unable to connect to git.freescale.com:
git.freescale.com: No address associated with hostname

how to resolve this?

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,045件の閲覧回数
johnnosky
Contributor I

FYI, anyone who comes across this now needs to go to the following link due to the shutdown of codeaurora.org:

https://github.com/nxp-imx/linux-imx.git

0 件の賞賛
返信

3,676件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Here is our git address:https://source.codeaurora.org/external/imx/linux-imx 

 

Best Regards

Zhiming

0 件の賞賛
返信