Unable to Capture Image on IMX8MM using imx334 Camera Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Capture Image on IMX8MM using imx334 Camera Sensor

1,707 Views
udhayamoorthi
Contributor II

I'm interfacing imx334 camera sensor on IMX8MM 

Following is the Register Log of Mipi Csi

Reading 0x48 count starting at address 0x32E30000

 

0x32E30000:  03060301 00004305 000F0000 DEADCAFE
0x32E30010:  F00FFFFF 00000000 00000000 00000000
0x32E30020:  00000000 0900001F DEADCAFE DEADCAFE
0x32E30030:  000001F4 00000000 00000000 00000000
0x32E30040:  000010B0 04380780 00000000 DEADCAFE
0x32E30050:  000008FD 80008000 00000000 DEADCAFE
0x32E30060:  000008FE 80008000 00000000 DEADCAFE
0x32E30070:  000008FF 80008000 00000000 DEADCAFE
0x32E30080:  000010B0 04380780 00000000 DEADCAFE
0x32E30090:  00000000 00000000 00000000 DEADCAFE
0x32E300A0:  00000000 00000000 00000000 DEADCAFE
0x32E300B0:  00000000 00000000 00000000 DEADCAFE
0x32E300C0:  00000000 00000000 6D111111 000000E4
0x32E300D0:  00000000 8E00802C 0000E579 DEADCAFE
0x32E300E0:  DEADCAFE DEADCAFE DEADCAFE DEADCAFE
0x32E300F0:  DEADCAFE DEADCAFE DEADCAFE DEADCAFE
0x32E30100:  000001C8 00000000 00000000 00000000
0x32E30110:  00000000 00000000 00000000 00000000

 

Following is the Register Log of CSI Bridge

 

Reading 0x48 count starting at address 0x32E20000

 

0x32E20000:  00020912 00000000 00000000 00000000
0x32E20010:  B602B6A8 00009600 80054001 00000000
0x32E20020:  00000000 00000000 00000000 00000000
0x32E20030:  00000000 028003C0 00000270 00000000
0x32E20040:  00000000 00000000 584AD030 00000010
0x32E20050:  00000000 00000000 00000000 00000000
0x32E20060:  00000000 00000000 00000000 00000000
0x32E20070:  00000000 00000000 00000000 00000000
0x32E20080:  00000000 00000000 00000000 00000000
0x32E20090:  00000000 00000000 00000000 00000000
0x32E200A0:  00000000 00000000 00000000 00000000
0x32E200B0:  00000000 00000000 00000000 00000000
0x32E200C0:  00000000 00000000 00000000 00000000
0x32E200D0:  00000000 00000000 00000000 00000000
0x32E200E0:  00000000 00000000 00000000 00000000
0x32E200F0:  00000000 00000000 00000000 00000000
0x32E20100:  00000000 00000000 00000000 00000000
0x32E20110:  00000000 00000000 00000000 00000000

 

According to this MIPI CSI is getting configured and also CSI Bridge is getting IMAGE DATA but CSI Bridge is not enabled and also SOF and EOF Interrupts are disabled .

When I try to Capture using V4L2 I get following 

#https://community.nxp.com/t5/i-MX-Processors/Can-t-able-to-get-V4l2-Sub-dev-in-imx8m-mini/m-p/15177...

Also there is no V4L2 subdevice and media0 in /dev  but I have video

and also when I try to capture it shows success in V4L2 IOCTL but does not give Image

#https://community.nxp.com/t5/i-MX-Processors/Can-t-able-to-get-the-raw-image-in-IMX8M-MINI/m-p/1519...

Attaching Dmesg Log , Device Tree and Driver Codes I'm using .

Don't know what I'm missing ? Pls try to help!

 

 

0 Kudos
Reply
0 Replies